SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-29T07:16:03-06:00SparkFun ElectronicsJonnerd on KIT-11943 - Cubelets - Bluetooth CubeletJonnerdurn:uuid:2cfd4339-0020-7229-a7f7-f8c73d6a3c452013-08-07T23:26:43-06:00<p>The Bluetooth Cubelet can actually do that. Although this product page talks only about Cubelets Control, Modrobotics has an API and programming environment called Cubelets Code that allows you to reprogram all of the other Cubelets using C. http://code.modrobotics.com and the API documentation is here: http://code.modrobotics.com/documentation/</p>
Ichbinjoe on KIT-11943 - Cubelets - Bluetooth CubeletIchbinjoeurn:uuid:c5503487-e52a-1cf3-9efd-4c22a06f5a302013-08-07T12:17:47-06:00<p>I think something along the lines of a 'controller' cubelet would be cool. Program it in like C or something with Microchip or Atmels libraries and send the program over the bluetooth to the controller. That would make this product line VERY cool. But then again, that would require a completely different way of the cubelets transferring data to each other. (More of an addressed method instead of 'static' like connections) Idk. Lots of ways the company that make cubelets could expand from here.</p>