SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T17:31:02-06:00SparkFun Electronicsmwwalk on PRT-12619 - SMD LED - Red 1206 (strip of 25)mwwalkurn:uuid:f7fda7ed-397c-96d9-e2b4-026aa83aeba52016-03-04T17:38:50-07:00<p>1) Thanks for carrying these, it's so annoying to have to put a seperate order in to digikey for only a few things like this.<p>2) I wish you'd carry more smd parts like these, especially in the 0805 size, which is the smallest my old eyes can work with.</p><p>3) I think these should be pretty bright at 120mcd. For maximum current, use a 150 ohm resistor for 5V or a 60 ohm resistor for 3.3V. Though personally, I'd just use a 330ohm.</p></p>