SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T06:46:31-06:00SparkFun ElectronicsCustomer #691629 on PRT-12842 - BeagleBone Black Enclosure - Clear PlasticCustomer #691629urn:uuid:8474b690-0ece-2c14-db86-a34dcc39d0072015-07-02T15:29:46-06:00<p>My case did not have this problem. You may want to ask for a replacement.</p>
Customer #691629 on PRT-12842 - BeagleBone Black Enclosure - Clear PlasticCustomer #691629urn:uuid:4da964b6-6621-4b6e-cd45-17cb1211da092015-07-02T15:28:47-06:00<p>I thought mine didn't come with a button pusher ("reset key") but it does, actually; it was wedged in the bottom of the box that the case came in.</p>
Customer #513455 on PRT-12842 - BeagleBone Black Enclosure - Clear PlasticCustomer #513455urn:uuid:a785e7d7-62c2-e518-ce97-2a95311109882015-01-30T10:15:37-07:00<p>Received this today and am very happy that it fits the Rev C and that no metal standoffs (or any standoffs) are required, the Beaglebone snaps into the bottom piece perfectly. I'm not as happy that the top of the case does not snap into place with the bottom, and requires tape to keep it securely closed. The description clearly says "...then snap the two sides together." But even though there are a total of 4 snap features (2 per side), they don't snap into the little holes that they are supposed to.<p>Despite this, I do like the flexibility of being able to more easily open the case to remove the Beaglebone board, rather than wresting with a clear and seamless edge, trying to break it out of its plastic jail.</p></p>
Jesse Craig on PRT-12842 - BeagleBone Black Enclosure - Clear PlasticJesse Craigurn:uuid:fee43497-ee0b-fa99-ccbb-1966803c61912014-09-16T19:28:13-06:00<p>I have had a lot of problems connecting to the HDMI and USB ports at the same time. The connectors on the two cables push against each other so much that the electrical connection is broken. Do you know of a good cable combo for using both ports at once?</p>
Nicolas Lebedenco on PRT-12842 - BeagleBone Black Enclosure - Clear PlasticNicolas Lebedencourn:uuid:786b943d-e87e-d57a-9742-26277d3851a82014-09-16T19:24:11-06:00<p>Well, I know it's been a long time and you have probably figured that out. Yes it fits, but the uHDMI connector and the USB Host ports are not well exposed. These ports remain some millimeters inside the plastic case making a huge difference for some connectors. With my HDMI cable for instance I couldn't get it attached to the uHDMI port up to the end. At first glance it looked connected though and before realizing there was a gap I went on a painful research on why my hdmi wasn't working...</p>
Jarryd on PRT-12842 - BeagleBone Black Enclosure - Clear PlasticJarrydurn:uuid:9b49d891-ac89-4c72-4048-1a2a623a96d92014-06-17T22:49:08-06:00<p>Just got mine today. Yes it fits both revision B and C.</p>
Jesse Craig on PRT-12842 - BeagleBone Black Enclosure - Clear PlasticJesse Craigurn:uuid:a926845a-9952-a085-917a-d0ef7d827dff2014-06-17T11:15:40-06:00<p>Yes, mine came with a button pusher.</p>
Jarryd on PRT-12842 - BeagleBone Black Enclosure - Clear PlasticJarrydurn:uuid:21fc6dd5-d329-f987-3374-5538750d856f2014-06-09T22:27:38-06:00<p>Does this also come with the button pusher you demonstrated on the Yun and Uno cases?</p>
Customer #559313 on PRT-12842 - BeagleBone Black Enclosure - Clear PlasticCustomer #559313urn:uuid:d1003741-d50e-381c-e2ad-0a829731a2cc2014-06-01T08:57:17-06:00<p>Also, can it fit a cape directly through the case? (CryptoCape for example?)</p>
Jesse Craig on PRT-12842 - BeagleBone Black Enclosure - Clear PlasticJesse Craigurn:uuid:c2808be5-712d-1a4a-596a-7212648e618d2014-05-26T07:30:06-06:00<p>Does this case fit the Rev C?</p>