SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-29T05:02:38-06:00SparkFun Electronicsazerimaker on WRL-13002 - Telescopic Antenna SMA - 75 MHz to 1 GHz (ANT500)azerimakerurn:uuid:dd912303-3dc0-22cb-5fcb-dcf438f1a2f12017-03-04T08:07:19-07:00<p>Hi, I want to buy Simultaneous RFID Reader - M6E Nano and use it with external antennas. In the hookup guide, there are some high-gain antennas mentioned, which are quite expensive and hard to find. I was wondering if I can use this antenna to read RFID tags from 2-3 meters?</p>