SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-18T22:00:42-06:00SparkFun ElectronicsSkerpy_D on COM-13004 - microSD USB ReaderSkerpy_Durn:uuid:b6b9ac40-6666-cf33-7a87-3c9485f9abe12014-09-20T18:40:06-06:00<p>When will this come back in stock? I back ordered one and I hope it gets here soon.</p>
Customer #587428 on COM-13004 - microSD USB ReaderCustomer #587428urn:uuid:af165a40-2d10-2281-c5ba-ab1013b46f472014-08-21T06:06:57-06:00<p>RobertC
you've stated it's SDXC, but the specs above only say SDHC. Are you sure it's SDXC capable?
thanks</p>
zshift on COM-13004 - microSD USB Readerzshifturn:uuid:db445862-03a4-60d6-4fe7-d716983a723b2014-08-15T19:34:25-06:00<p>This is awesomely tiny.</p>
RobertC. on COM-13004 - microSD USB ReaderRobertC.urn:uuid:d7cea3a1-c00d-741e-547b-e448746fddb92014-08-15T10:57:02-06:00<p>this is an SDXC, which means extended capacity. which apparently <a href="http://en.wikipedia.org/wiki/Secure_Digital#SDXC" rel="nofollow">supports cards up to 2TB</a></p>
Customer #260321 on COM-13004 - microSD USB ReaderCustomer #260321urn:uuid:55f3a3a6-6b9a-a837-3ef1-9aa8ac60a61a2014-08-15T10:54:43-06:00<p>What capacity & class will this handle? Some SD readers only go up to 2GB, others max out at 32GB.</p>
Nate on COM-13004 - microSD USB ReaderNateurn:uuid:6b668e66-bed2-cda4-3a17-c9f2631285e72014-08-15T09:50:37-06:00<p>It's capable of full read/write.</p>
Customer #469299 on COM-13004 - microSD USB ReaderCustomer #469299urn:uuid:5ad86c31-455b-456b-5d2c-79eaae9043032014-08-15T09:28:47-06:00<p>When plugged into the computer, can I write to the micro SD card, or, as the description strongly suggests, this is a read-only solution?</p>
LightManCA on COM-13004 - microSD USB ReaderLightManCAurn:uuid:2c0c4101-2a42-4416-09d5-7075ee7f993b2014-08-14T18:02:40-06:00<p>Wow I'll have to include that in my next order!</p>