SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T09:31:06-06:00SparkFun ElectronicsCF on PRT-13112 - E-Textiles Battery - 110mAh (2C Discharge)CFurn:uuid:88f71b51-c31b-d3a8-43ce-b5b70d82c1fe2018-02-15T14:39:07-07:00<p>Hello!
Most charges are meant to be used with a larger battery than these. You need a charger that can be set for 100mA charging. We carry one that will work with this battery called the <a href="https://www.sparkfun.com/products/14380" rel="nofollow">Adjustable LiPo Charger</a>. Just set the DIP switch for 100 and you should be all set.</p>
Arcyepes on PRT-13112 - E-Textiles Battery - 110mAh (2C Discharge)Arcyepesurn:uuid:c337e67f-3ab9-52e9-71f9-cd9549f153ea2018-02-15T13:10:01-07:00<p>I bought some of these. I have the SparkFun basic LiPo charger. When I plug in, the light turns off and seems to not charge anymore. Is there a way to find out if it is charging? if not then what charger do I need?I can charge other Lipo batteries just fine. I'm assuming it has something to do with the protection board the battery comes with. Please help</p>
Customer #820351 on PRT-13112 - E-Textiles Battery - 110mAh (2C Discharge)Customer #820351urn:uuid:fbb2c985-286a-e934-a9f3-36bbdb2cef642018-01-22T14:27:47-07:00<p>What is the mass of the battery? Unfortunately, it is not in the datasheet.</p>
Customer #139760 on PRT-13112 - E-Textiles Battery - 110mAh (2C Discharge)Customer #139760urn:uuid:759dce01-cd57-8cb2-7c56-5e5c0d7525b82016-12-05T05:08:57-07:00<p>Curious what type of "specialized Lithium Polymer Charger" will work. I got 2 of these batteries and couldn't charge them with a LiPo charger from Adafruit (https://www.adafruit.com/product/1944). Could someone please give some examples of suitable chargers?</p>
pattyl on PRT-13112 - E-Textiles Battery - 110mAh (2C Discharge)pattylurn:uuid:7f8d4282-7933-c65a-0050-adc321c3c7512015-02-25T17:49:18-07:00<p>I bought the SparkFun LiPo Charger Basic - Micro-USB - PRT-10217 - to charge the 110mA battery, but the status light will not go on. When I charge the 400mA LiPo, the status light is on and I presume the battery is charging. Any suggestions on how to charge the 110mA battery? I have the USB/microUSB cable connected to a USB port on my laptop, which tech support said should work.</p>
IgnacioV on PRT-13112 - E-Textiles Battery - 110mAh (2C Discharge)IgnacioVurn:uuid:cfed8229-2e4a-649a-548f-80e6dd24bebf2014-12-21T11:43:02-07:00<p>It would not be that surprising to find a 4C or higher discharge rate on the regular ones.</p>
PointyOintment on PRT-13112 - E-Textiles Battery - 110mAh (2C Discharge)PointyOintmenturn:uuid:96c99237-000e-982d-f14d-97d88273fd402014-12-15T21:25:42-07:00<p>The regular version of this battery doesn't seem to specify a discharge rate, so it's hard to compare them.</p>
jkbgbr on PRT-13112 - E-Textiles Battery - 110mAh (2C Discharge)jkbgbrurn:uuid:38da7561-9d51-5ca8-cf44-b9fc5bf50adc2014-12-15T14:05:17-07:00<p>Could you give a value to the extreme lightness? I'm considering to use it on a device attached to a bird - weight really does matter for me.</p>