SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T17:14:17-06:00SparkFun ElectronicsCustomer #1364955 on DEV-13883 - LilyPad Coin Cell Battery Holder - Switched - 20mmCustomer #1364955urn:uuid:57e66bf1-05db-3f6f-d858-4ab9e8ecd6632018-04-28T12:02:50-06:00<p>Overall dimensions? 3D models? I'm kind of surprised that one or both of these aren't here on the product page. I think I managed to figure it out on my own, but it'd be nice to have some of this readily available.</p>
M-Short on DEV-13883 - LilyPad Coin Cell Battery Holder - Switched - 20mmM-Shorturn:uuid:77e117c0-02bd-6195-af94-384cf7c844de2016-10-12T09:23:47-06:00<p>According to the <a href="http://cdn.sparkfun.com/datasheets/Prototyping/BAT-BLH-001.jpg" rel="nofollow">datasheet</a> the battery holder is 4.2mm. The PCBs are 0.8mm. You probably want to add in a bit since the battery holder isn't flush with the board and does have a bit of solder under it, but it should be about 5mm.</p>
jfadams on DEV-13883 - LilyPad Coin Cell Battery Holder - Switched - 20mmjfadamsurn:uuid:615c9a18-870e-a688-36b8-ae70f1331faf2016-10-12T01:17:33-06:00<p>Anyone know how thick this is (bottom of board to top of battery holder)?</p>
Customer #848168 on DEV-13883 - LilyPad Coin Cell Battery Holder - Switched - 20mmCustomer #848168urn:uuid:5d7d9d32-14ee-fed9-3680-0c348d2896ff2016-09-28T08:50:34-06:00<p>Is this hand washable without batteries?</p>