SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T20:13:33-06:00SparkFun Electronicssantaimpersonator on COM-14139 - Sewable LED Ribbon - 1m, 50 LEDs (White)santaimpersonatorurn:uuid:5f4e476e-9d64-497f-9a84-0ad6b80259812019-04-25T12:02:24-06:00<p>Yes, it looks like it is a pair of wires with LEDs tied in parallel.</p>
KaGe_Diver on COM-14139 - Sewable LED Ribbon - 1m, 50 LEDs (White)KaGe_Diverurn:uuid:ab7507d7-2e99-d902-59f8-a69f7d592d4c2019-04-25T10:49:39-06:00<p>Can these be joined together for a longer section? Can they be trimmed to length?</p>
ericjforman on COM-14139 - Sewable LED Ribbon - 1m, 50 LEDs (White)ericjformanurn:uuid:b11c4204-b9e0-7517-3ed0-6247a3a662492017-07-01T08:15:06-06:00<p>Can you post a photo of the 360-degree LED strip taken out of the fabric? Video showcase, and datasheet, doesn't show it clearly. Curious how it's achieved, through lens or refraction or extra LEDs?<p>Also, would like to know if possible to source these without the fabric. The manufacturer website (www.inolux-corp.com) has no information on it.</p></p>