SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T16:39:08-06:00SparkFun ElectronicsEternityForest on SPX-14293 - Qwiic Mux - PCA9548AEternityForesturn:uuid:cf2ba068-ca18-a940-9927-c8039155b0f92018-06-02T00:03:16-06:00<p>Does this provide 5v power via a Qwiic connector?<p>If so, maybe there should be a little symbol that makes the 5V one more obvious, if you're gonna use the same connector for 5v stuff, or maybe a switch or a jumper should be required to enable 5v output.</p><p>You could even have a "5v is on" LED!</p></p>