SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T15:29:44-06:00SparkFun Electronicsjohn luke on TOL-14508 - Slice Craft Knifejohn lukeurn:uuid:f5f916ed-28dd-0efb-157b-c58c3d59d3922018-01-05T18:22:41-07:00<p>I bought one of these in the hope that a ceramic blade would be super sharp. In practice though the
blades seem quite dull. Not sharp enough to cut open the pack of replacement blades. I had to fall back
to my trusty $2 snap off blade box cutter which was much sharper. So for me steel is sharper.<p>Will have to buy some steel blades to make uses of this expensive device. I regret buying the
replacement blades which seem no sharper.</p></p>
elijahparker on TOL-14508 - Slice Craft Knifeelijahparkerurn:uuid:98de29ef-cc0d-f106-80a7-b19f6135438a2017-12-15T11:23:32-07:00<p>Awesome, thanks for the reply! I'll probably try it out.</p>
One Chris Two Chris Red Chris Blue Chris on TOL-14508 - Slice Craft KnifeOne Chris Two Chris Red Chris Blue Chrisurn:uuid:52f6babd-1e7e-7dd7-3268-124fc8af0c1f2017-12-15T10:39:24-07:00<p>Great questions! I have found that these blades are just as sharp and cut as smooth as steel, but yes they are a bit frailer on the lateral movement. Now that being said, I was a bit surprised by how little the difference between the two was in terms of breakage point.<p>You can see an example of it cutting in the video for this product. Hope this helps!</p></p>
elijahparker on TOL-14508 - Slice Craft Knifeelijahparkerurn:uuid:c80031fd-154b-31e2-15bc-6c582074210b2017-12-15T09:27:54-07:00<p>Looks nice but I have a couple questions: Are these as sharp and cut as smoothly and cleanly as steel blades? I like the idea but don't want a sub-par cut. Also, are they prone to breaking from lateral force or can they flex a little? Thanks!</p>