SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T20:19:03-06:00SparkFun Electronicssantaimpersonator on SEN-14725 - eYs3D Stereo Camera - EX8036santaimpersonatorurn:uuid:b9ae8ccf-f4d7-4fac-4f5d-bbd787c0f7392020-08-01T02:08:09-06:00<p>I am not sure if we are allowed to have that posted. However, you can reach out to our TS team on the <a href="https://forum.sparkfun.com/" rel="nofollow">forums</a>. They will do their best to assist you, if possible.</p>
Customer #158122 on SEN-14725 - eYs3D Stereo Camera - EX8036Customer #158122urn:uuid:2a5dce20-e843-663d-634f-c114fd2e4fab2020-07-27T15:40:57-06:00<p>Got the camera but the box got thrown out. Can someone post the FTP site info here?</p>
CF on SEN-14725 - eYs3D Stereo Camera - EX8036CFurn:uuid:d55f326f-134f-fff9-5677-0dcd57af81642020-03-03T12:07:43-07:00<p>The paper in the box has a FTP site to visit along with a username and password. You need to visit that FTP site and log in with the username and password on the paper to download files for this product.</p>
Customer #1577493 on SEN-14725 - eYs3D Stereo Camera - EX8036Customer #1577493urn:uuid:dcd5b463-f458-170d-de4a-5b109641aa812020-02-12T22:04:01-07:00<p>I bought this product, but where should I download the viewer?
There is no download link in the box.</p>
Customer #1462217 on SEN-14725 - eYs3D Stereo Camera - EX8036Customer #1462217urn:uuid:ebcf6313-de5e-3dd5-41a3-59056b60a5182018-12-17T14:12:01-07:00<p>Yes, the software tool comes with this feature. You can set the color depth display range between 12.5 cm to 1638.4 cm (~ 0.4 ft to 54 ft) or anything in between. In your case, you can set the range from 61 cm to 91 cm, approx (2 to 3 ft).</p>
Customer #331485 on SEN-14725 - eYs3D Stereo Camera - EX8036Customer #331485urn:uuid:624203ab-0148-8aba-0e35-220157d499bf2018-12-15T08:56:18-07:00<p>Can I set the depth range that I want to sense distance? For example can I set it so that the full color depth range falls within distance say between 2 and 3 feet from the camera, meaning the depth range to be sensed is only one foot of depth?</p>
Customer #1462217 on SEN-14725 - eYs3D Stereo Camera - EX8036Customer #1462217urn:uuid:959fcf73-98ef-ee09-118d-b230c170c71a2018-11-17T06:45:08-07:00<p>This camera output with depth+color information which is possible for 3D scanner application.</p>
Customer #1462217 on SEN-14725 - eYs3D Stereo Camera - EX8036Customer #1462217urn:uuid:f0fd5364-19a8-8384-a182-9286b66de1592018-11-17T06:43:26-07:00<p>The correct datasheet has updated, thanks!</p>
lgrfbs on SEN-14725 - eYs3D Stereo Camera - EX8036lgrfbsurn:uuid:c3f77d7d-f349-149f-e103-b8811827dda82018-11-17T01:12:50-07:00<p>Can this camera be used in a 3D scanner?</p>
Chinwah on SEN-14725 - eYs3D Stereo Camera - EX8036Chinwahurn:uuid:6d5bdd54-6936-13e0-3151-e20a829428e42018-11-17T00:59:36-07:00<p>Appears that the data sheet is incorrect for this module. Mechanical drawings and pictures in the data sheet dont match the Sparkfun pictures.</p>
Customer #1462217 on SEN-14725 - eYs3D Stereo Camera - EX8036Customer #1462217urn:uuid:44779390-9f96-0646-e981-3426e4d14fdf2018-11-16T14:41:53-07:00<p>The close limit is around 15 cm. Depth accuracy <3% within 1 M or <10% within 3.5 M depends on system requirement.</p>
Customer #115158 on SEN-14725 - eYs3D Stereo Camera - EX8036Customer #115158urn:uuid:ac990539-bdd8-8899-cefd-6905ce0247552018-11-16T14:27:31-07:00<p>What are the approximate close and far limits on the depth sensing range?</p>
One Chris Two Chris Red Chris Blue Chris on SEN-14725 - eYs3D Stereo Camera - EX8036One Chris Two Chris Red Chris Blue Chrisurn:uuid:a6abc08b-ef57-ae84-169a-066e5c7290f12018-11-16T09:25:18-07:00<p>Unfortunately, this camera is <em>not</em> waterproof.</p>
Customer #310431 on SEN-14725 - eYs3D Stereo Camera - EX8036Customer #310431urn:uuid:8317bf6f-76e6-e112-8157-835cd3b71daa2018-11-16T08:43:48-07:00<p>Is it waterproof?</p>