SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T23:08:48-06:00SparkFun ElectronicsCustomer #1462217 on SEN-14726 - eYs3D Stereo Camera - EX8029Customer #1462217urn:uuid:1f263e20-dbad-b51b-c6d4-87a1d1c3f0192018-11-07T20:19:34-07:00<p>Unfortunately a ROS driver is not available at this moment.</p>
Customer #1462217 on SEN-14726 - eYs3D Stereo Camera - EX8029Customer #1462217urn:uuid:b2464ea1-f70d-c7af-4b33-1c2c0a00bb8f2018-11-07T20:15:31-07:00<p>Potentially any objects within the range of measurable distance, depend on distance from objects to camera lens. Please check the datasheet 1.3 (Figure3) on depth accuracy.</p>
Customer #1462217 on SEN-14726 - eYs3D Stereo Camera - EX8029Customer #1462217urn:uuid:2e6251b8-1651-57d9-6614-eac3938f2ab52018-11-07T20:11:25-07:00<p>No, the camera alone does not support 3D or VR-3D streaming, although it's possible with additional camera modules and image post processing.</p>
Customer #487217 on SEN-14726 - eYs3D Stereo Camera - EX8029Customer #487217urn:uuid:54c130bf-9ea5-9541-2bbf-6aac5e1bb5062018-11-07T12:34:23-07:00<p>Can I use the camera to stream 3D video on YouTube or similar?</p>
lgrfbs on SEN-14726 - eYs3D Stereo Camera - EX8029lgrfbsurn:uuid:147261db-69c8-7175-61fe-0d91498bc15d2018-11-06T08:35:47-07:00<p>If I want to build a 3d scaner of this product.
What size/type of items can I expect that the Scaner will work well with?
* Model Railroad in scale 1:87
* Food Plate
* Foot Baths
* Small Car
* Truck
* Steam locomotive
* IORE locomotive?
* Airplane</p>
dbc on SEN-14726 - eYs3D Stereo Camera - EX8029dbcurn:uuid:fd69deee-a952-92b5-de73-4d2846ad1e242018-11-04T16:55:27-07:00<p>Actually, I was asking if a ROS driver was available to publish depth data -- a ROS driver would sit on top of UVC. A typical depth camera ROS driver would publish a point cloud on a ROS topic.</p>
Customer #1462217 on SEN-14726 - eYs3D Stereo Camera - EX8029Customer #1462217urn:uuid:c5619cc4-9ae8-a1d3-d5ee-0fbe08ec8a002018-11-03T06:09:19-06:00<p>Camera net weight is around 25.5g.</p>
Customer #1462893 on SEN-14726 - eYs3D Stereo Camera - EX8029Customer #1462893urn:uuid:19df4267-493d-1653-a6a2-e4656d6eeb6f2018-10-31T17:18:28-06:00<p>How much does this camera weigh?</p>
Customer #1462217 on SEN-14726 - eYs3D Stereo Camera - EX8029Customer #1462217urn:uuid:f483bbee-6994-80af-ea85-2cbeff5594492018-10-30T19:30:20-06:00<p>Yes, EX8029 can detect distance farther than 300cm but with less accuracy.</p>
Customer #1462217 on SEN-14726 - eYs3D Stereo Camera - EX8029Customer #1462217urn:uuid:e1ac6a4a-616e-40a6-0b87-00cd82c2c4062018-10-30T19:29:41-06:00<p>Yes, the stereo camera (EX8029) is UVC compliant and does not require any ROS driver.</p>
dbc on SEN-14726 - eYs3D Stereo Camera - EX8029dbcurn:uuid:d5b94c5e-5328-c6b1-343e-c600d55895012018-10-28T21:13:27-06:00<p>Do the USB enpoints appear as UVC devices? Is there a ROS driver?</p>
Customer #259001 on SEN-14726 - eYs3D Stereo Camera - EX8029Customer #259001urn:uuid:c2645ae4-b581-9f6e-8e9b-e7965cee95322018-10-26T11:55:11-06:00<p>This looks a good alternative to Kinect 1.<p>Does it have a specification on max sensing distance? There is only a delta accuracy chart up to 300cm. Will it still work beyond that or just worse accuracy?</p></p>