SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-29T01:28:42-06:00SparkFun ElectronicsCustomer #631347 on WRL-15007 - Serial Telemetry Radio Kit - 915MHz, 100mWCustomer #631347urn:uuid:e3519732-91ec-cd38-7270-d0884facda312020-05-20T10:21:11-06:00<p>In your 2018 product showcase video Pete asked the public to let you guys know if there was interest in this item. Now that you carry the 100mW version, any plans to add the 500mW version to your store front? Thanks</p>
santaimpersonator on WRL-15007 - Serial Telemetry Radio Kit - 915MHz, 100mWsantaimpersonatorurn:uuid:0de06551-1086-3998-f488-602e26e6628c2020-04-29T20:02:36-06:00<p>Unfortunately, we don't have any product in to check. However, this question might be best directed at the manufacturer, as it might not be labeled on the enclosure anyways: productservice@holybro.com</p>
chip on WRL-15007 - Serial Telemetry Radio Kit - 915MHz, 100mWchipurn:uuid:96c0c3e9-b7dc-7c8a-f6aa-2294efb416eb2020-04-21T09:07:21-06:00<p>Do these radios have an FCC ID?</p>
Customer #436035 on WRL-15007 - Serial Telemetry Radio Kit - 915MHz, 100mWCustomer #436035urn:uuid:a8f87328-ce5d-f909-96d4-f1dddb506e762019-09-14T03:15:25-06:00<p>I'm facing similar issues when trying to use this set with GPS-RTK2 board. Have you found a solution to this problem yet?</p>
Customer #24015 on WRL-15007 - Serial Telemetry Radio Kit - 915MHz, 100mWCustomer #24015urn:uuid:9afa8381-347d-e6a0-d819-cac0c71f2b612019-04-06T21:12:19-06:00<p>I was hoping I could just use this as a transparent serial link. I'm looking for a simple way to send RTCM data from one "SparkFun GPS-RTK Board - NEO-M8P-2" board (basestation) to another (rover) as an RTK setup. So when I connect the USB cables to a PC and it enumerates a virtual COM port then I can send serial data at 57600 baud from one HyperTerminal session to another - nice! When I'm sending this data, on a single Radio Module I hook up an O-scope to both the TX and RX pins and I see that both are outputting 3.3V serial data. I would have expected one to be an input and the other an output. Not both as outputs. I get the same result if I use the USB port just to power the Radio Modules through a USB power wart - both are outputs. Does this make sense?</p>