SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T18:25:13-06:00SparkFun ElectronicsCustomer #752003 on COM-15206 - LED RGB Strip - Addressable, Bare, 1m (APA104)Customer #752003urn:uuid:d9d1c81d-6f23-b9f4-fa21-c5b4d844349d2021-08-18T09:48:40-06:00<p>I'm late to the party but yes, you can easily cut these strips. Those black lines are exactly where you want to cut them, that leaves enough of the contact pad on each side to solder to.</p>
Customer #1651349 on COM-15206 - LED RGB Strip - Addressable, Bare, 1m (APA104)Customer #1651349urn:uuid:5490615b-22ac-ba03-94d4-56bd5d34b3fa2021-01-23T17:46:27-07:00<p>Hi! I would love to use this for a personal project but the length is far too long to use. I was wondering if it were possible to cut the strip a foot in or so and be able to access the wires in the middle. From the picture, there are black lines which may indicate a good spot to cut between the LEDs. Thank you!</p>