SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T08:00:09-06:00SparkFun ElectronicsCustomer #704271 on SPX-15586 - Qwiic SwitchCustomer #704271urn:uuid:f28ee47d-2fac-dbc6-8fa9-f0878dfa162d2021-02-26T01:47:00-07:00<p>Buyer beware! Read my review. The FIFO queue functionality of the sparkfun/Qwiic_Button firmware is broken. This bug was reported six months ago and is still not fixed. There's no way to access queued button press and button click timestamps (other than the first and last) without it.</p>
santaimpersonator on SPX-15586 - Qwiic Switchsantaimpersonatorurn:uuid:0e4a3356-375b-7562-74ff-64d37bd510f22019-12-18T17:41:26-07:00<p>I'll follow up with the SparkX team, it seems a general use version and/or a toggle switch would be useful.</p>
djbyter on SPX-15586 - Qwiic Switchdjbyterurn:uuid:5c21efdd-52b5-beb8-aa8a-d22679cd20b82019-12-10T10:21:15-07:00<p>Some suggestions, after installing 30 of these:<ul>
<li><p>I've broken 3 of them so far due to the actual switch pads coming off the board. I feel like you could make those pads slightly bigger (and whatever it takes so it doesn't lift off the board) and that would help greatly.</p></li>
<li><p>I've been using these also with toggles, but it requires a bit of jimmy rigging. If there were another hole to fit <a href="https://www.sparkfun.com/products/9276" rel="nofollow">these</a> or <a href="https://www.sparkfun.com/products/11310" rel="nofollow">these</a> that would be nice</p></li>
<li><p>The tiny sliver of board on the far side feels like it wants to snap off. I know it's not connected, it's just used for anchoring but if that was slightly wider then it wouldn't feel like it's so fragile.</p></li>
</ul></p>
djbyter on SPX-15586 - Qwiic Switchdjbyterurn:uuid:4958b094-107d-d46b-bce5-e07157b697202019-11-22T13:40:37-07:00<blockquote>
<p>https://www.sparkfun.com/products/11310</p>
<p>I'm about to try and use this for these actually, would it not work right off the bat? Looks like this is designed for a momentary switch, but with code like <code>button.isPressed()</code> - wouldn't that just work without changes?</p></blockquote>
Red Squirrel on SPX-15586 - Qwiic SwitchRed Squirrelurn:uuid:02d55e6c-f9ba-854a-1d4e-1354af42de112019-11-09T13:04:26-07:00<p>Nice! Could you make one for these? https://www.sparkfun.com/products/11310</p>
santaimpersonator on SPX-15586 - Qwiic Switchsantaimpersonatorurn:uuid:ea9e6bff-075e-4f4a-705b-9b3ec56f93732019-08-19T10:50:10-06:00<p>I believe I saw them building more... I would check back again just in case or you can also backorder them.</p>
Customer #134773 on SPX-15586 - Qwiic SwitchCustomer #134773urn:uuid:8641611f-e42b-39e4-6f41-f1535e1d0a7d2019-08-16T21:04:50-06:00<p>Drat... they're all gone! Sure hope this one makes it to a "regular" product!</p>
santaimpersonator on SPX-15586 - Qwiic Switchsantaimpersonatorurn:uuid:d4f6b254-4ec0-5746-d04e-3741a754924a2019-08-13T17:04:42-06:00<p>Hey there, sorry about that.<ul>
<li>I'll try to get the schematic uploaded again. (<em>We are currently experiencing some server issues; we are working to repair links/recover files.</em>)</li>
<li>The GitHub repository was still private. It should be public now and the link should be working.</li>
</ul></p>
mariof on SPX-15586 - Qwiic Switchmariofurn:uuid:57f62980-3de9-f84b-64c1-08592859f3d12019-08-13T07:09:19-06:00<p>The Schematic and Hardware Repo links are not working..</p>
Customer #134773 on SPX-15586 - Qwiic SwitchCustomer #134773urn:uuid:7e6e4ca2-faa4-27e6-42b4-0df1264a26bb2019-08-13T01:08:02-06:00<p>Yay! Almost feels like an instance of "ask and ye shall receive!" ;-)</p>