SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T05:46:28-06:00SparkFun ElectronicsOne Chris Two Chris Red Chris Blue Chris on DEV-16271 - NVIDIA Jetson Nano Developer Kit (V3)One Chris Two Chris Red Chris Blue Chrisurn:uuid:3bbd15af-8d78-be67-b571-cd1360faa76e2020-09-20T02:32:24-06:00<p>Yes, you are correct!</p>
nanogear on DEV-16271 - NVIDIA Jetson Nano Developer Kit (V3)nanogearurn:uuid:967008e4-6e49-2c02-581b-ba32a6490a5d2020-09-18T13:04:23-06:00<p>hello!! The V3 is the newest version of Jetson Nano nowadays?</p>
santaimpersonator on DEV-16271 - NVIDIA Jetson Nano Developer Kit (V3)santaimpersonatorurn:uuid:c8115992-a8e5-3761-13d9-05a1d647a9502020-01-28T18:17:10-07:00<p>Unfortunately, I wasn't quite sure what @CrustyCarbuncle was trying to point out. That being said, there wasn't version 2 (V2) of the carrier board; however, I believe that we do highlight the primary change to the carrier board:<blockquote>
<p>"This version of the Jetson Nano Developer Kit comes equipped with two MIPI-CSI camera connectors which enables algorithms that perform stereo vision!"</p>
</blockquote><p>To clarify for all customers, <strong>the Xavier module does not come with this kit</strong>. The product name specifies the Jetson Nano specifically and as specified under the <strong>Includes</strong> tab, only the carrier board is the third revision:</p><blockquote>
<p>"NVIDIA Jetson Nano Module and Carrier Board (V3)".</p>
</blockquote></p>
santaimpersonator on DEV-16271 - NVIDIA Jetson Nano Developer Kit (V3)santaimpersonatorurn:uuid:177e89f0-f014-8b73-bd0a-b25653968a8f2020-01-28T18:03:12-07:00<p>The carrier board is supposed to be forward compatible with the unreleased Xavier module and as specified under the <strong>Includes</strong> tab, the Jetson Nano module is included in this kit: "NVIDIA Jetson Nano Module and Carrier Board (V3)".<p>Unfortunately, I'm not sure how to interpret the rest of your comment. Could you rephrase for me?</p></p>
PhilG on DEV-16271 - NVIDIA Jetson Nano Developer Kit (V3)PhilGurn:uuid:94b6b190-10d8-325b-0e19-6b00983141b92020-01-17T10:38:14-07:00<p>This page needs some details as to the difference between V2 and V3. As Crusty points out, this doesn't appear to be the newly released Xavier NX module which comes with:<p>384-core NVIDIA Volta @ 1100MHz with 48 Tensor Cores</p></p>
CrustyCarbuncle on DEV-16271 - NVIDIA Jetson Nano Developer Kit (V3)CrustyCarbuncleurn:uuid:9144d40c-7071-771c-5e7d-011cfb1534612020-01-17T09:59:21-07:00<p>I gather that though these boards support the Nano 'production' and the new Xavier modules, they are being supplied with the earlier, non-'production' Nano modules. The main (only?) difference is the presence of the 16 Gb eMMC modules on the production modules.<p>Is this correct?</p></p>