SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T12:18:41-06:00SparkFun Electronicsdpitchfo on PRT-16890 - Board to Board Double Slot Female Connector - 50 pin, 0.5mm dpitchfourn:uuid:f463c5b0-8048-c1a4-d693-60fd772495f22023-09-19T14:00:31-06:00<p>Looking at the datasheet for the the male connector (PRT-16890), the drawing is miss leading for the PCB Layout. The embossed alignment hole is on the wrong side. If you look at the side view, it shows the correct location for the emboss pin, but the schematic view needs to be rotated 180 degrees.</p>
dpitchfo on PRT-16890 - Board to Board Double Slot Female Connector - 50 pin, 0.5mm dpitchfourn:uuid:c507e69c-04ac-3f9d-872c-a1fb4a7749cb2023-08-30T10:24:13-06:00<p>The link to the drawing for the connector is not working.</p>