SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T12:11:46-06:00SparkFun ElectronicsWimL on WRL-17506 - SparkFun LoRa Thing Plus - expLoRaBLEWimLurn:uuid:06e1c4a7-ac80-5c5f-eea7-123140ce3e7a2022-05-24T22:10:04-06:00<p>How much current does this draw while idle? Or, does anyone have numbers on how long it can last per battery charge with different levels of activity?</p>
santaimpersonator on WRL-17506 - SparkFun LoRa Thing Plus - expLoRaBLEsantaimpersonatorurn:uuid:006a6713-e695-913e-528b-54339bd26b7d2021-10-19T14:08:28-06:00<p>As mentioned in the banner above, please refer to the <a href="https://www.sparkfun.com/technical_assistance" rel="nofollow">technical assistance page</a> for details on <a href="https://forum.sparkfun.com/" rel="nofollow">posting on our forum</a>.<p>Based on the library, <code>setDataMode</code> is only called when <a href="https://github.com/sparkfun/SparkFun_ADXL313_Arduino_Library/blob/master/src/SparkFunADXL313.cpp#L71-L78" rel="nofollow">SPI is used to communicate with the ADXL313</a>. My guess is that the issue is in your code, if you are connecting to the sensor with a Qwiic cable <em>(i.e. SPI is not the same as I2C)</em>.</p></p>
santaimpersonator on WRL-17506 - SparkFun LoRa Thing Plus - expLoRaBLEsantaimpersonatorurn:uuid:dbf93017-d7ca-b3b1-f273-8b1b45c5062b2021-10-19T14:01:13-06:00<p>No this board is not a Qwiic peripheral device; it has a SiP with an Apollo3 microcontroller and SX1262 LoRa module. Currently, the microcontroller itself doesn't support Python.</p>
BamBam on WRL-17506 - SparkFun LoRa Thing Plus - expLoRaBLEBamBamurn:uuid:82b62cec-8b2b-0a6a-3c80-89e268d3cc9e2021-09-22T12:54:41-06:00<p>So I bought this development board to use the Qwicc connect system alongside ADXL313 breakout boards, but it seems as if the Sparkfun ADXL313 library is not compatible with this board as the compiler gives a "setDataMode" error can someone point me in the correct direction to make this work?</p>
ElephantHat on WRL-17506 - SparkFun LoRa Thing Plus - expLoRaBLEElephantHaturn:uuid:272cc485-5097-8f26-fec8-6c0c01eadc092021-04-27T13:50:29-06:00<p>Is there any example code for setting up the board with Python? And if not are there any plans? It seems like the qwiic devices all have python examples so I would love to use python with the main board as well.</p>