SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T23:35:08-06:00SparkFun ElectronicsCustomer #1711220 on SPX-17522 - Qwiic IR Thermometer - MLX90614Customer #1711220urn:uuid:0065f292-032a-d1ab-7b98-d8ed3b97a1012022-03-14T03:54:31-06:00<p>the code is not for ESP32. I have the same problem with my SparkFun Thing Plus - ESP32 WROOM and SparkFun Thing Plus - ESP32 WROOM (U.FL)- The code works only for RED Board QWIIC or Plus</p>
Customer #1711220 on SPX-17522 - Qwiic IR Thermometer - MLX90614Customer #1711220urn:uuid:24d9fea4-936e-d75f-560b-ae361369596e2022-03-14T03:50:20-06:00<p>the GitHub link that you post in Documents doesn't work</p>
Customer #393665 on SPX-17522 - Qwiic IR Thermometer - MLX90614Customer #393665urn:uuid:42f21008-4512-e4c8-9d24-fceee26a47812022-01-15T16:24:57-07:00<p>I find the MLX90614 sensor useful and reliable but had the same problems itemized below with this board coupled to a new ESP32 Thing Plus. Code will not compile. Reverted to a previous SF non-QWIIC breakout board of the same sensor, connected standard I2C wires on the board end, QWIIC on the bus end, used the Adafruit library, everything worked.</p>
Customer #322428 on SPX-17522 - Qwiic IR Thermometer - MLX90614Customer #322428urn:uuid:d372c210-9450-7b2c-8c99-75c88ae7997e2021-01-31T17:16:12-07:00<p>Beware, the Arduino library and MKR devices do not appear to work with this board. The address is 5A vice 3A, and even after changing to this value, does not appear to return a valid value. I checked the device with a Pi 4 board, and a short python script; it worked. Not sure what's going on with the Arduino lib and MKRs.</p>
Customer #1634836 on SPX-17522 - Qwiic IR Thermometer - MLX90614Customer #1634836urn:uuid:45442b0a-77df-0d38-8faa-ab6697498b4b2020-12-16T07:59:34-07:00<p>The Get_Temperature example code worked great with a Redboard Qwiic board over a qwiic i2c connection, but when I tried the same code with a Artemis Thing Plus over a qwiic i2c connection, it didn't print any temperature readings in the serial monitor. It just printed "Qwiic IR Thermometer did acknowledge." in the serial with the Artemis Thing Plus. I did make sure I had the correct board and com port selected in the Arduino IDE.</p>