SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T07:09:32-06:00SparkFun Electronicscmdailey on PRT-17752 - Argon ONE M.2 Raspberry Pi 4 Casecmdaileyurn:uuid:c8105d05-bf07-5bf1-bd4e-04a40e4a9eb92021-01-22T22:30:24-07:00<p>It looks like SparkFun just picked my my absolute favorite Pi4 case on the market. I've been using this particular case for a few months now, and it has absolutely delivered on everything I wanted. The fan plus top metal of the case works as an amazing cooling solution (to the point that the fan nearly never even needs to run with all the heat dissipated by the case,) the ease of slapping in an m.2 sata drive and booting up has increased my boot speeds as much as it has my happiness.<p>It's well built, sturdily made, and looks absolutely slick. The dust cover (magnetic!) for the GPIO ports is way cool, and makes it feel like your Pi is always ready to tinker if you want, or to look like a micro pc if you don't.</p><p>I can't recommend more for the price!</p></p>