SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-29T07:27:35-06:00SparkFun Electronicstulgee on COM-18000 - SparkFun QwiicBus - MidPointtulgeeurn:uuid:43313203-21ca-4fb4-8641-2ca0af93a8812024-01-13T09:46:03-07:00<p>It would be nice to see this redone with the ethernet jacks rotated 90 degrees. It would be a whole lot easier to protect your project in a box if you could make one hole in one side rather than try to figure out how to make this weird design work.</p>
Customer #1668110 on COM-18000 - SparkFun QwiicBus - MidPointCustomer #1668110urn:uuid:435c4d09-7739-f431-095d-4de83af1e66c2021-04-19T22:09:42-06:00<p>Can this "midpoint" be directly connected to the Raspberry Pi and used as a t-connector? What I need is to use it as a "T-splitter" so I can send 2 cables with sensors in 2 different directions away from the Pi, and then use the QwiicBus EndPoints at the ends of both cables. Is it possible to use this board in this manner? Thank you.</p>