SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T23:21:41-06:00SparkFun Electronicstetsujin on CAB-21271 - SparkFun 4-in-1 Multi-USB Cable - USB-C Hosttetsujinurn:uuid:69a96481-b015-b4ec-8cef-36ad81e238542023-12-13T15:26:24-07:00<p>I have to wonder if a type-B connector on the end is really the right choice at this point. I still have some 20 year old devices kicking around with B-type receptacles on them, but I feel like most people have never even seen a USB-B connector at this point.
Perhaps an A-type receptacle would be a better choice if you change the cable in a future revision? There's still loads of stuff using A-type plugs, causing some frustration for people with laptops that mostly just have C-type receptacles.</p>
Will2 on CAB-21271 - SparkFun 4-in-1 Multi-USB Cable - USB-C HostWill2urn:uuid:070efb04-169a-2f95-f8b9-1ff85e061cde2023-03-19T11:52:55-06:00<p>Pay attention to the "max 500 mA" note at the end. This is not a charging cable.</p>