SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-29T08:58:04-06:00SparkFun ElectronicsJeraz on DEV-00032 - 40 Pin AVR Development Board w/USB ConnectionJerazurn:uuid:baedc471-279f-0873-da36-fa1dfa1f00ca2013-01-17T14:46:16-07:00<p>will the sparkfun AVR pocket programmer be able to program this board through the ICSP port?</p>
MacWire on DEV-00032 - 40 Pin AVR Development Board w/USB ConnectionMacWireurn:uuid:e92e2f19-39dc-93a6-5c85-a50a71a665632010-07-08T17:13:58-06:00<p>There's no pull-up on the i2c clock (see schematic). You have to add one in yourself to get the eeprom working. Other than that, the board works great.<br>
I used it with ATMEGA16PU and 24LC256.</p>