SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T12:59:42-06:00SparkFun ElectronicsToni_K on DEV-00037 - Development Terminal - ATMega128Toni_Kurn:uuid:bd7b9bca-22dc-b7c3-03db-b037d2fc1fac2011-04-06T12:02:08-06:00<p>Yes it does.</p>
Digisynth on DEV-00037 - Development Terminal - ATMega128Digisynthurn:uuid:9a67efbb-5306-c3b7-3377-75ef784297372011-04-04T11:58:51-06:00<p>Does this board come fully assembled?</p>
PaulS. on DEV-00037 - Development Terminal - ATMega128PaulS.urn:uuid:613134d6-4777-23c6-81f2-88286ff3c2452010-05-14T19:26:44-06:00<p>Figured it out, thanks.. :)<br>
I didn't realize I needed a programmer on the rs232, also. I ended up using the JTAG-USB programmer. Works great!</p>
Pearce on DEV-00037 - Development Terminal - ATMega128Pearceurn:uuid:91751ad0-47d6-00e2-8152-0d4f0e4dbd7b2010-05-14T15:51:56-06:00<p>check with us at tech support, we might be able to help you out.</p>
PaulS. on DEV-00037 - Development Terminal - ATMega128PaulS.urn:uuid:5a0cdd02-2f80-45bd-6045-8b1a975e15272010-05-12T15:15:20-06:00<p>Has anyone managed to connect to this board via the built-in serial port? I can't for the life of me get it connected in Windows (avrdude and AVR Studio) or Mac OS (crosspack/avrdude).</p>
Jordii on DEV-00037 - Development Terminal - ATMega128Jordiiurn:uuid:dad0be80-b5c9-f1c2-1b7d-13a6d648917a2009-05-16T12:10:50-06:00<p>A good source code of the board is found here:<br>
<a href="http://olimex.com/dev/soft/avr/Atmega128_MT-WINAVR.zip" rel="nofollow">http://olimex.com/dev/soft/avr/Atmega128_MT-WINAVR.zip</a><br>
Includes all the functions to interface with all the hardware, including the LCD.<br>
Jordi Munoz</p>