SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-29T04:15:50-06:00SparkFun Electronicstoddfun on BOB-00497 - SparkFun SSOP to DIP Adapter - 8-Pintoddfunurn:uuid:b3a87a33-7e19-de3b-0bb2-502f2191434e2016-02-10T10:57:14-07:00<p>I have the same issues ad RobBrownNZ with Crystal Oscillator Driver (http://www.ti.com/lit/ds/symlink/sn74lvc1404.pdf) SN74LVC1404<p>I don't see why you wouldn't bring the pads in more so narrow parts with 0.65mm pitch could still use the breakout board. I will have to go someplace else I guess. :(</p></p>
mguirg on BOB-00497 - SparkFun SSOP to DIP Adapter - 8-Pinmguirgurn:uuid:53fc5996-4254-970a-ef75-fac6ae637b7d2011-04-08T19:52:26-06:00<p>Will these work for an 8-pin opamp. Like an LM471?</p>
Mr. Cruz on BOB-00497 - SparkFun SSOP to DIP Adapter - 8-PinMr. Cruzurn:uuid:3468cb87-4335-a98b-c527-4b0e970262f62011-04-02T12:49:05-06:00<p>Yes, I have just soldered a MSOP package onto this board.<br>
Remember, Flux is your friend.</p>
RobBrownNZ on BOB-00497 - SparkFun SSOP to DIP Adapter - 8-PinRobBrownNZurn:uuid:7cc207bd-8b75-0c6b-0526-1482507e9c672011-02-11T02:29:14-07:00<p>I have some devices (SN74LVC2T45 level converters, http://focus.ti.com/lit/ds/sces516i/sces516i.pdf) that are 0.65mm pitch but the total width is only 4mm (3.75mm minimum). I can't find an adapter to fit them! If you revise this board, would you please consider making them to fit narrower packages?<br>
Also, I think they're too expensive. I guess the price comes from them being small and fiddly, but perhaps you could make them cheaper by making them in a strip of (say) 10 that are not completely routed out from each other? Believe me, I think that SparkFun's prices are generally really good but I just think these little adapter boards are an exception :)</p>
ErikP on BOB-00497 - SparkFun SSOP to DIP Adapter - 8-PinErikPurn:uuid:1ad335e9-df4d-91a3-b295-9deee2874ef12011-01-19T14:47:26-07:00<p>Yes, these should work with MSOP-8. Since these SMT pads are so long, the width across the IC body is not very critical and so this can handle several different package types as long as the pin pitch is 0.65 mm (or very close)</p>
Customer #40537 on BOB-00497 - SparkFun SSOP to DIP Adapter - 8-PinCustomer #40537urn:uuid:81ef4e31-dbbe-88b4-351d-7152c697fac62010-12-09T13:15:03-07:00<p>So, will these work on MSOP-8???</p>
N.Poole on BOB-00497 - SparkFun SSOP to DIP Adapter - 8-PinN.Pooleurn:uuid:00c117c9-261d-5207-90f1-dbfaabf927e92010-11-14T02:06:09-07:00<p>...Oh...<br>
look over there, SOT23 breakouts...<br>
Hahahahahahaha...<br>
well at least I got the wrong thing to work right! lmao!</p>
N.Poole on BOB-00497 - SparkFun SSOP to DIP Adapter - 8-PinN.Pooleurn:uuid:1ede198d-d769-1785-6658-95df9d2ee5402010-11-11T18:05:49-07:00<p>I now know that you can slap an SC70 on here... if you do it creatively:<br>
<a href="http://i600.photobucket.com/albums/tt82/TheRiggingCellar/workaroundSOIC.jpg" rel="nofollow">http://i600.photobucket.com/albums/tt82/TheRiggingCellar/workaroundSOIC.jpg</a></p>
Chris917 on BOB-00497 - SparkFun SSOP to DIP Adapter - 8-PinChris917urn:uuid:7f74fbb9-e32f-bcc2-9532-9729cf8392fd2010-05-16T16:41:18-06:00<p>Will these work for msop-8?</p>