SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T10:23:16-06:00SparkFun ElectronicsRitch on SEN-00638 - CMOS Camera Module - 640x480 - SMD ConnectorRitchurn:uuid:4eda5617-f2e8-c6fe-648a-4dd5eda584f22010-03-30T06:17:38-06:00<p>I recently had a mishap with my Samsung Tocco F480 and being me I've whipped it apart. The dual camera setup is linked with this SMD connector type but it has 34-pins not 20. The screen also has a 34-pin connector and as the touchscreen is included it woud seem like a fun project. Do you have 34 pin versions of this connector?</p>