SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T03:47:24-06:00SparkFun ElectronicsCustomer #390467 on CEL-00757 - GM862 Cellular Quad Band ModuleCustomer #390467urn:uuid:07b4f97a-e528-83cc-b63a-4b3655fafd112013-01-21T13:21:50-07:00<p>Is there compatible breakout board that sparksfun currently sell?</p>
Klone38 on CEL-00757 - GM862 Cellular Quad Band ModuleKlone38urn:uuid:35edeefd-f3b9-300c-7e64-333e82b371792010-11-25T17:27:42-07:00<p>Is this the same module that you use in your Port-O-Rotary phones?</p>
haroldo on CEL-00757 - GM862 Cellular Quad Band Moduleharoldourn:uuid:b1adaa0c-7a23-a056-684f-9553b58b98802010-10-26T14:41:58-06:00<p>I'm working with Uber Board and naw, I arrived on the part of GM862 and I'd like to know if to communicate with it, we have to put any code, like the Bluetooth. Because, we set the MUX to cell module, send power pulse, and after, what we have to do?<br>
PLEASE, could somebody help me?<br>
my e-mail is: jhcbj@hotmail.com<br>
sorry for the wrong english</p>
johnnyfive on CEL-00757 - GM862 Cellular Quad Band Modulejohnnyfiveurn:uuid:26640ada-6010-f011-d875-d7f38cce369b2010-09-08T15:11:23-06:00<p>Not to rain on SparkFun's parade (love this site!) but you can get the updated GM862-PY(THON SUPPORT!) for $80 here: <a href="http://www.semiconductorstore.com/cart/pc/viewPrd.asp?idproduct=42834#details" rel="nofollow">http://www.semiconductorstore.com/cart/pc/viewPrd.asp?idproduct=42834#details</a><br>
I'd rather buy it from SparkFun, but no way i'm going to buy an older module with less functionality for more.</p>
ik on CEL-00757 - GM862 Cellular Quad Band Moduleikurn:uuid:e0adaa5f-c1ad-4e68-e0b2-d34b3615811f2010-02-27T22:15:18-07:00<p>A viola is a bowed string instrument.</p>
rlv on CEL-00757 - GM862 Cellular Quad Band Modulerlvurn:uuid:80107bb1-fbf3-47a2-577e-a16aff312ccf2009-07-22T23:20:30-06:00<p>I also would like to know if SparkFun could provide the GM862-QUAD-PY version of this module. The ability to run python code in the chip makes it possible to eliminate a microcontroller in my design, and simply connect SPI devices to gather inputs.<br>
Unfortunately, looking at the dates of the older posts makes is look pretty lonely here in the comment section.<br>
One vendor for the GM862-QUAD-PY appears to be trenz-electronic.de for about $135 US.</p>
richms on CEL-00757 - GM862 Cellular Quad Band Modulerichmsurn:uuid:9dc302f6-6729-6a5e-e458-8c2e9fc703b12009-01-31T06:11:25-07:00<p>Are there any UMTS versions of these going to be available?<br>
Also can these handle all the connecting to the APN and stuff and just present as a serial port a connection to a remote IP address?</p>
ComNile on CEL-00757 - GM862 Cellular Quad Band ModuleComNileurn:uuid:fecf53d4-e6e6-3977-efad-770093af8ad42009-01-12T02:46:16-07:00<p>Is this module (GM862 Cellular Quad Band Module) in this site support python scripts or not,it's essential to know before i buy it, as i saw in telit site two different modules(The GM862-QUAD) and the (The GM862-QUAD-PY), which one is this.thanks</p>