SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T11:05:59-06:00SparkFun ElectronicsCustomer #525777 on DEV-07830 - Ethernet Web PIC Development BoardCustomer #525777urn:uuid:7fb2ae25-db1c-2ff6-9a75-a142ad7bdcb52014-03-06T21:34:50-07:00<p>Hello,
how can I connect this board to
Edimax EW-7811Un 150 Mbps Wireless 11n Nano Size USB Adapter with EZmax Setup Wizard
Edimax EW-7811Un 150 Mbps.
I can add a USB port to this board if I have to, or is there an easier way
I need to have the wifi internet connection
Thanks and regards<p>Kazem</p></p>
RobertC. on DEV-07830 - Ethernet Web PIC Development BoardRobertC.urn:uuid:bb28428d-9abb-4c6d-11ed-55da12656ead2012-11-06T16:43:17-07:00<p>it seems there are some patches. I think the issue is that Olimex keeps changing the rev on us without letting us know, so there tends to be confusion with which product people actually are getting. I'm getting the product page updated right now to make sure we have all the documentation listed here appropriately. plenty of people have gotten the board to work over the years, I think documentation here is the main issue.<p>Does that help at all? As always, tech support can help you further on a more technical level.</p></p>
Toni_K on DEV-07830 - Ethernet Web PIC Development BoardToni_Kurn:uuid:9ea7d7db-8d9e-12b1-e85a-c9b6c78aaa312012-11-06T16:08:27-07:00<p>Actually, it's a good link, just bad formatting. Find the actual page <a href="http://datrus.com/picweb-howto.html" rel="nofollow">here</a>.</p>
Customer #120710 on DEV-07830 - Ethernet Web PIC Development BoardCustomer #120710urn:uuid:a64dcf4b-e7af-75b0-44b8-937742f128da2012-11-02T13:17:40-06:00<p>To Sparkfun Product Manager: After looking at all of the above and comments about patches, etc., it does not inspire confidence. Does this product work right out of the box or does the developer have to recompile, reconfigure and whatever just to get it to read a simple serial port?</p>
LloydA on DEV-07830 - Ethernet Web PIC Development BoardLloydAurn:uuid:4f7fffe1-09f3-5255-4fc5-26340d56045d2012-10-31T13:37:32-06:00<p>Troll link. Internet Archive shows that the entire time the site existed it was nothing more than a 404 page.</p>
S2H69 on DEV-07830 - Ethernet Web PIC Development BoardS2H69urn:uuid:4f692d58-a96f-11fb-b865-76bcc3d220c22011-08-03T15:38:22-06:00<p>A really handy board if you want to get something online at a low cost. Little bit of trouble getting Olimex's patch onto Microchip's TCPIP stack working (try contacting Olimex directly, and they might send you a patched version of the stack).<br>
The only problem that I encountered was noise on all ADC channels whenever there is network traffic. Not sure if other people have seen this, but keep an eye out for it!</p>
rand1 on DEV-07830 - Ethernet Web PIC Development Boardrand1urn:uuid:baecc555-87c1-4aaa-fd6c-28d7c7a6dd112011-03-13T13:36:16-06:00<p>Will I be able to use the PIC-PG1 to program this board? It is the PIC18F67J60, this chip isn't listed in the ICPROG program. Anything else compatible? Open source solutions? The PIC-PG1 says it works "with all Olimex PIC Development boards", so it's electrically correct? Any suggestions are appreciated.</p>
Moetz on DEV-07830 - Ethernet Web PIC Development BoardMoetzurn:uuid:9cd0b290-5c9f-0f8e-f6c5-d4c04a2568a32010-02-27T05:52:36-07:00<p>Hope you are able to answer this!<br>
I would actually like to know how the webpages could be uploaded on the Pic Web rev.b. I tried ftp both via client program and through browser and I even tried using the Hyperterminal in Win and it didn't work either.<br>
Are the webpages suposed to be uploaded into the micro as a hex file instead of using the mentioned image files that was suposed to be uploaded to the onboard eeprom. Apparently this eeprom does not exist on the rev.b as far as I can see.????</p>
raygeeknyc on DEV-07830 - Ethernet Web PIC Development Boardraygeeknycurn:uuid:090cbd6c-ab26-7acc-d6c7-71f71f1131c02010-02-19T21:37:06-07:00<p>I have a successfully patched TCP/IP stack for the rev.B boards - contact me (PM on the Forum] if you need a copy and cannot get it. [FYI -- The patch that Olimex supplies does not work with the currently posted TCP/IP stack from Microchip]</p>
bokubob on DEV-07830 - Ethernet Web PIC Development Boardbokuboburn:uuid:c069071b-f8c4-a87f-9b3a-1ae7155189812010-02-02T07:28:44-07:00<p>SparkFun's description lists a "Power plug-in jack for +5VDC power supply" however the board requires more than 5VDC. See the documentation for the proper specs.</p>
Blue Hair Bob on DEV-07830 - Ethernet Web PIC Development BoardBlue Hair Boburn:uuid:bdd0b93f-125f-5bfd-ab63-34acb15804132010-01-20T17:51:03-07:00<p>The description for this needs to be updated and we need links to the current documents. The rev B board doesn't have an ENC28J60 on it, does it?</p>
raygeeknyc on DEV-07830 - Ethernet Web PIC Development Boardraygeeknycurn:uuid:aafb3485-179b-1dba-82de-df4b6eea08e72010-01-16T23:32:04-07:00<p>Does anyone have the rev.B board working? I cannot get the patch applied and in the forum, no one seems to be able to.</p>
Saib30 on DEV-07830 - Ethernet Web PIC Development BoardSaib30urn:uuid:5984726c-912d-e5bf-855f-5fdbbf246f792009-05-28T01:37:24-06:00<p>Please not that PIN 18 on the EXT connector (referred to as EXT-18) is connected to the 5V and not 3.3V as stated in the schematic.</p>
MarcMTL on DEV-07830 - Ethernet Web PIC Development BoardMarcMTLurn:uuid:c8b03842-4a5f-0b86-724a-ee6fdebda4ee2009-05-19T21:08:54-06:00<p>Here is a project I implemented using the Olimex PIC-WEB Board:<br>
<a href="http://www.mgdengineering.com/hvac.htm" rel="nofollow">http://www.mgdengineering.com/hvac.htm</a><br>
Really great to work with, reliable and good documentation on Olimex's part.<br>
Marc</p>
Cole on DEV-07830 - Ethernet Web PIC Development BoardColeurn:uuid:6a456426-8df0-698d-ab75-cf42f1df91262009-04-02T17:32:34-06:00<p>Here is a must have document for interfacing with this board.<br>
<a href="http://www.olimex.com/dev/pdf/PIC/Understanding-PIC-WEB-boards.pdf" rel="nofollow">http://www.olimex.com/dev/pdf/PIC/Understanding-PIC-WEB-boards.pdf</a></p>
Jonathon Cox on DEV-07830 - Ethernet Web PIC Development BoardJonathon Coxurn:uuid:cdf2480b-c46a-faea-f9e1-953638b00eaf2008-12-08T01:51:16-07:00<p>This is a really good site for linux users<br>
<a href="http://datrus.com/picweb-howto.html" rel="nofollow">http://datrus.com/picweb</a></p>