SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T11:21:32-06:00SparkFun Electronicsstevenvh17 on BOB-07841 - SparkFun USB to FIFO Breakout - FT245RLstevenvh17urn:uuid:afbce6c5-ce36-d952-cd96-588b187e6e872015-01-28T01:10:49-07:00<p>I agree that it would be more handy to have the pinout printed at the top side, but the reason why it's printed on the bottom is probably a simple one: there's more space there.</p>
stevenvh17 on BOB-07841 - SparkFun USB to FIFO Breakout - FT245RLstevenvh17urn:uuid:53cf482f-9ae7-7baf-041e-23b3af6097eb2015-01-27T10:13:20-07:00<p>FTW, 1.5x0.92" = 38.1 mm x 23.4 mm. Metric, for Pete's sake.<p>Except that this can't be right. There are 9 holes at 2.54 mm pitch, so the total board length is about 10 x 2.54 mm, or 25.4 mm (1"), certainly not 1.5".</p></p>
stevenvh17 on BOB-07841 - SparkFun USB to FIFO Breakout - FT245RLstevenvh17urn:uuid:0866af19-1ea4-d7f3-67ea-16351f51910f2015-01-22T11:48:28-07:00<p>I was wondering the same thing. According to https://www.riecktron.co.za/en/image/cache/data/products/07841-01-600x600.jpg it's a mini USB.<p>Sparkfun, can the next version of this BOB be with a micro-USB connector? Mini-USB is so passé.</p></p>
Customer #450512 on BOB-07841 - SparkFun USB to FIFO Breakout - FT245RLCustomer #450512urn:uuid:7ad8a3ca-024f-b98d-9fe9-f5432fe119282015-01-04T01:53:07-07:00<p>i can't tell from the photos: does this use mini usb or micro usb? also, can this be used for implementing an HID device recognized by a pc/mac/linux box as a HID device without a driver install? also, this thing is multiple years old…is it on its way out? is there a better option here for what i'd like to do?</p>
Kamiquasi on BOB-07841 - SparkFun USB to FIFO Breakout - FT245RLKamiquasiurn:uuid:dac55924-c5aa-4326-a55b-28f83e2637d32012-10-24T05:29:48-06:00<p>If you mean the SparkFun schematic of the actual board - I think what's going on is that they're showing the I/O pins as 1 'header' JP1, with the VCCIO pin separate on the single pin JP3.<p>JP2 is also 8 pins, which does seem incorrect, but all that's missing is the 2nd GND pin which is connected to the first one on the board.. not a huge problem :)</p></p>
Customer #372555 on BOB-07841 - SparkFun USB to FIFO Breakout - FT245RLCustomer #372555urn:uuid:458d9caf-ef13-08d3-84a8-e81a7994d9852012-10-24T05:22:28-06:00<p>It looks that also the schematic is not correct.
It shows 8 pin on the header as the board has 9 pins header.</p>
Kamiquasi on BOB-07841 - SparkFun USB to FIFO Breakout - FT245RLKamiquasiurn:uuid:8101983d-e7d0-4ccf-5d8b-73643770670f2012-10-23T16:31:42-06:00<p>If you're using Eagle CAD, try this <a href="http://www.filedropper.com/fpbob07841" rel="nofollow">BOB-07841 Footprint, Eagle v5.11 library file</a><p>If not, you can manually space it: <a href="http://i.imgur.com/dPZLn.png" rel="nofollow">Screenshot, 0.1" grid</a></p></p>
Customer #372555 on BOB-07841 - SparkFun USB to FIFO Breakout - FT245RLCustomer #372555urn:uuid:66ecd47d-4cf5-a29f-b3d9-868ed996bfad2012-10-23T14:06:37-06:00<p>I have to put it on a other PCB. Where can i find the footprint?</p>
Customer #345108 on BOB-07841 - SparkFun USB to FIFO Breakout - FT245RLCustomer #345108urn:uuid:0b7769fd-24b6-9850-29fd-c8f84d501ea82012-08-11T04:39:41-06:00<p>Guys I want to Know whether interfacing Keyboard with Microcontroller is Possible with Break out Board (USB to Parallel Converter,FT245R)...Please post your ideas...</p>
gchristopher on BOB-07841 - SparkFun USB to FIFO Breakout - FT245RLgchristopherurn:uuid:f10a2646-1afd-eb3e-058b-ab555b859ec12011-11-18T15:39:07-07:00<p>I found this really easy to get started using. I downloaded a sample C++ project from the FTDIChip-ID Examples section of the website, started adding code from the D2XX Programmer's Guide document, and it's working great.</p>
RogerInHawaii on BOB-07841 - SparkFun USB to FIFO Breakout - FT245RLRogerInHawaiiurn:uuid:da913b71-eb00-a048-c56d-a680b2f90cf12011-09-26T16:17:38-06:00<p>Do you have any sample code you can share (ideally, C# code)? I'm having lots of trouble figuring this thing out.</p>
RogerInHawaii on BOB-07841 - SparkFun USB to FIFO Breakout - FT245RLRogerInHawaiiurn:uuid:782fc865-f3ab-1d87-1ba7-2b6c07669d762011-09-26T16:16:14-06:00<p>I'm finding this incredibly difficult to implement. It would really help if there were sample code (particularly C# sample code) for this product. I've read through a lot of documentation on the FTDI website, and I've successfully installed the drivers, but cannot find examples or instructions on how to actually USE it from a C# program. Any help would be greatly appreciated.</p>
Customer #209620 on BOB-07841 - SparkFun USB to FIFO Breakout - FT245RLCustomer #209620urn:uuid:0b990360-cf56-4752-a394-861b0a5ace372011-03-22T09:00:43-06:00<p>I'm wondering if you could use this with an iphone/ipod to pull the audio signals out - any ideas?</p>
MoeHoward on BOB-07841 - SparkFun USB to FIFO Breakout - FT245RLMoeHowardurn:uuid:eede1b0b-c971-3045-1d2a-dd1d2d12304c2011-02-08T21:44:43-07:00<p>Tip for the next version of this breakout board: "Put the pin label silk screen on the top of the device and not on the bottom of the board."<br>
The first thing someone will do is put headers on this breakout board and use it on a breadboard, then guess what, they will need to pull it out and look on the underside to confirm pin outs. Seems like a simple design idea, not sure how this item slipped by. I am sure there is a reason for it, right?</p>
ryxxui on BOB-07841 - SparkFun USB to FIFO Breakout - FT245RLryxxuiurn:uuid:6979157a-3c05-f706-ceb4-eaa174df65af2010-03-26T12:15:48-06:00<p>This board is really awesome. You can use it to send or receive data to any system- I have an ATMega328p functioning as a latch and simple controller for the signals.<br>
There is only one problem though, and I'm not sure who's end it is on. I know that my circuit is correct, as well as my code (cocky but I've checked this many, many times). However, my data is being scrambled at some point. I'm not sure if it's a problem with how Windows is sending the data, or a problem involved in the pin labelling, but the data I am sending is showing up in the wrong order on the data output pins. Still, as long as you test your circuit before you have gotten to a point where this is difficult to get around, this board and chip are an awesome and simple way to send data to a system over a USB connection.</p>
r1c@1v@r3z on BOB-07841 - SparkFun USB to FIFO Breakout - FT245RLr1c@1v@r3zurn:uuid:5e60ee12-8c47-be84-072d-d1570a9fc8352009-09-27T19:08:22-06:00<p>v1.05 datasheet link is broken, returns 404 error.<br>
V2.06 is now available at <a href="http://www.ftdichip.com/Documents/DataSheets/DS_FT245R_V206.pdf" rel="nofollow">http://www.ftdichip.com/Documents/DataSheets/DS_FT245R_V206.pdf</a>.<br>
Can you verify that the new datasheet is consistent with the FT245R on this board?<br>
thanks</p>