SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T17:15:29-06:00SparkFun ElectronicsCustomer #202770 on DEV-08353 - PICAXE-28X Starter PackCustomer #202770urn:uuid:8d6d147a-8c56-1ecf-5bf2-6a4868110ed62011-03-03T20:20:15-07:00<p>I was wondering if you can put a 28x2 on this development board?</p>
Customer #158394 on DEV-08353 - PICAXE-28X Starter PackCustomer #158394urn:uuid:13a1a90c-b2d3-f2f7-9395-01fd2425fdf02010-12-18T11:33:03-07:00<p>On this board, if you use the 754410 (L293D) motor drive chip in the socket provided, the inputs and outputs are reversed to that shown in the manual. Motor A is Motor B and Pin 5 is pin 6 on the diagram etc. If you just mirror all the pins and motors its works just fine. Otherwise a great board for development work.</p>
I2C Master on DEV-08353 - PICAXE-28X Starter PackI2C Masterurn:uuid:3fed6d9a-06d2-041d-e547-cd572fe6634a2009-12-02T19:07:01-07:00<p>Uh, SparkFun can you just make a new prouduct. You could just include the PICAXE 28X1 IC, unassembled 28-pin standard project board, and project board. If you do not want the Software CD and Interface cables. I would by one on the 2009 "Free Day," pleeeeeeeeeeeeeeeeeeeeeese!</p>