SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-29T08:20:32-06:00SparkFun ElectronicsCustomer #1353727 on SEN-08505 - Ultrasonic Transducer - Maxbotix UTCustomer #1353727urn:uuid:539a7ea5-0f1b-7065-7e35-e2a75b08a7b52018-04-15T07:58:38-06:00<p>How can we connect 300 KHz transceiver to Arduino. please help</p>
rocketblast on SEN-08505 - Ultrasonic Transducer - Maxbotix UTrocketblasturn:uuid:93c37c03-2444-83e9-aa6a-8b4f1286f8652011-06-09T21:35:36-06:00<p>Do you what the angle of the sound cone is. For example If a second transducer is 1m in front and I begin to move it side ways, at what distance will it stop picking up the first transducer?</p>
disabelle on SEN-08505 - Ultrasonic Transducer - Maxbotix UTdisabelleurn:uuid:59148d59-86a5-3ebb-7aba-783c537519d92011-05-29T19:18:33-06:00<p>whats the pin out can u upload more pictures to show that would be very helpful</p>
disabelle on SEN-08505 - Ultrasonic Transducer - Maxbotix UTdisabelleurn:uuid:8e95486c-5278-04ec-3dc3-0423ff34ffed2011-04-27T23:38:55-06:00<p>how far can it sense in feet im hoping about 5-10ft?<br>
and what would i use to boost the sensor? if needed to i wanna save money and buy just the sensor not with the board under it like the break out board. sorry im new to this.</p>
Andrew12 on SEN-08505 - Ultrasonic Transducer - Maxbotix UTAndrew12urn:uuid:097e4df8-9cfb-8aa8-ef7a-befc012d0d112011-01-09T10:22:22-07:00<p>http://en.wikipedia.org/wiki/Ultrasonic_sensor.<br>
Long story short - its a two-way transducer.</p>
majolsurf on SEN-08505 - Ultrasonic Transducer - Maxbotix UTmajolsurfurn:uuid:585a916a-0455-bee6-c4b6-c49cffbc7ac72010-08-27T02:32:58-06:00<p>I was pretty surprised at the sensitivity of this transducer.<br>
You can transmit and receive from the same module. Check out the following link for a simple sonic ranger project featuring this transducer...<br>
<a href="http://majolsurf.net/wordpress/?page_id=829" rel="nofollow">http://majolsurf.net/wordpress/?page_id=829</a></p>
Conrthomas on SEN-08505 - Ultrasonic Transducer - Maxbotix UTConrthomasurn:uuid:f0ac27bf-3510-c818-827f-c25c0f7eee912010-07-14T11:05:52-06:00<p>This is basically a stripped down version of the other maxbotix boards. It is only the transducer. Therefore, with the correct supporting circuitry (see the datasheets on other maxbotix sensors for examples) it should be able to act as the other send-receive-measure sensors. Hope that helps.</p>
Ninja0n3 on SEN-08505 - Ultrasonic Transducer - Maxbotix UTNinja0n3urn:uuid:3d85bfe5-277c-1d27-488a-dce318f93bfa2010-05-23T01:21:54-06:00<p>Does this device allow me to both send and receive an ultrasonic wave or does it just produce the sound?<br>
What device would I need to get in order to just receive an ultrasonic wave if this doesn't do it?</p>