SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-29T00:36:27-06:00SparkFun ElectronicsCustomer #32913 on DEV-08557 - Ethernet Micro Web DeviceCustomer #32913urn:uuid:815f3981-c555-6c6e-3a0a-cef4c6986c052011-03-17T09:57:38-06:00<p>On the TCP/IP stack, answer is must be old 5.00 version, new ones will not work. Microchip does not have old one, here is link:<br>
http://rapidshare.com/files/283549509/TcpStack-500.rar</p>
Customer #32913 on DEV-08557 - Ethernet Micro Web DeviceCustomer #32913urn:uuid:f7704fc7-1460-2aa4-8435-4b1ebbb785fb2011-03-16T16:15:40-06:00<p>Hi, just received board and it works fine communicating to it via web. Olimex documentation says there is a configuration web page but does not give address. Does anyone know?<br>
Also, I have tried their step by step instructions to patch TCP/IP stack by Microchip, I just get long list of errors (about 50% successful). Any clues? Finally, can not find any tech support contact from Olimex. Thanks for your help.</p>
maf on DEV-08557 - Ethernet Micro Web Devicemafurn:uuid:c0d3d28f-cd1c-f4e4-9514-a7fe3eddfaf62011-03-06T20:27:58-07:00<p>The Ubiquiti Network INSTANT 802.3af Adapter will work with an 802.3af switch to power the PIC-MICRO-WEB. It's listed as supporting 16V, .8A (12.8W), enough for the module without any additional components.</p>
xcvbfsghrtytry on DEV-08557 - Ethernet Micro Web Devicexcvbfsghrtytryurn:uuid:01419165-4fe1-0064-9189-4b47316956252010-04-27T11:35:41-06:00<p>To use with standard POE, a 25K resistor between pins 7 and 8 will tell the switch to turn on the power.</p>
xcvbfsghrtytry on DEV-08557 - Ethernet Micro Web Devicexcvbfsghrtytryurn:uuid:b85db62a-19e5-95f4-f92f-90ac430cdf1f2010-04-27T10:23:49-06:00<p>Are these not IEEE802.3af or IEEE802.3at compliant? My POE switch does not seem to want to power them on.</p>
syzygy on DEV-08557 - Ethernet Micro Web Devicesyzygyurn:uuid:861a9d11-0da9-aa4f-1255-cb016402ee5b2010-01-03T18:13:06-07:00<p>Looks like it directly mentions the ICSP so I'm guessing no</p>
syzygy on DEV-08557 - Ethernet Micro Web Devicesyzygyurn:uuid:58182cde-913e-7b28-8a19-5b1ece5ae8da2010-01-03T18:10:25-07:00<p>Does this come with any type of bootloader pre-installed?</p>