SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T20:30:06-06:00SparkFun ElectronicsHarinath on GPS-08622 - 20 Channel GS405 Helical GPS Receiver ConnectorHarinathurn:uuid:3056599c-beb4-81ee-6b03-059540d0202b2012-06-07T00:19:37-06:00<p>Hello sparkfun, I can't find 10 pin ( 2 rows ) SWD jumper here. This is very useful for people who are working on ARM microcontrollers.
Please stock them. Below are the few links where you can see the connector.
SAMTEC shrouded header: FTSH-105-01-F-D-K<p>http://www.samtec.com/ftppub/pdf/FTSH_MT.PDF</p><p>http://www.samtec.com/ftppub/pdf/FTSH_SMT.PDF
For more details see here :
http://www.keil.com/support/man/docs/ulink2/ulink2_hw_connectors.htm</p><p>http://support.code-red-tech.com/CodeRedWiki/HardwareDebugConnections</p><p>This 10 pin male connector occupies less space than JTAG.</p></p>
MattAttack on GPS-08622 - 20 Channel GS405 Helical GPS Receiver ConnectorMattAttackurn:uuid:7bf3c040-2684-dc2e-9d61-e904bd1102ae2010-01-13T08:43:18-07:00<p>Be careful if you use this on a breakout board! The bent over surface mounting ends of the pins can short to the metal case on the GPS module when it is pressed in. I ended up using a through hole part (DigiKey p/n S9015E-05-ND) on my breakout board.</p>
I Heart Robotics on GPS-08622 - 20 Channel GS405 Helical GPS Receiver ConnectorI Heart Roboticsurn:uuid:20d44fc3-3f29-ee68-29e4-8c31f86eee5d2008-11-30T17:31:36-07:00<p>The pins on this connector are slightly too long. The data sheet specifies a length of 2mm as opposed to 4.5mm for the mating area.<br>
On the other hand this does give you some room for double stick tatpe to secure the receiver.</p>