SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T11:04:22-06:00SparkFun ElectronicsAristarco on PRT-08631 - RCA JackAristarcourn:uuid:309ad656-caa4-607f-9578-f8e4884947d52015-02-20T09:05:18-07:00<p>I'll join my voice to those asking for the White and Red versions. Painting this one just looks FUGLY.</p>
jjt on PRT-08631 - RCA Jackjjturn:uuid:abd7e53a-37bf-0090-3dca-39ee342c64622013-08-05T16:13:41-06:00<p>It's also wrong in Eagle.</p>
jjt on PRT-08631 - RCA Jackjjturn:uuid:0f72437c-ce8f-49f5-cb56-7d265e2782c22013-08-05T14:58:36-06:00<p>The schematic for this part in the July 27 Fritzing release shows the switching between the ground (pin 1) and pin 3, when the switch is between pins 3 and 2. And SF should also carry these in RED and WHITE, yellow is specifically for video in the AV universe.</p>
bitsmashed on PRT-08631 - RCA Jackbitsmashedurn:uuid:5205a529-6094-2ed4-a24f-9f38625211662011-12-05T14:41:01-07:00<p>Sorry for the super late response, but it's under POWER_JACKRCA.</p>
scooter_seh on PRT-08631 - RCA Jackscooter_sehurn:uuid:c6175801-a766-d42a-5fd6-ec2fa41461162011-04-16T21:03:01-06:00<p>Anyone have a part file for fritzing?</p>
Digisynth on PRT-08631 - RCA JackDigisynthurn:uuid:fd8db67f-6683-229b-00af-78de1d4710af2011-01-13T16:12:21-07:00<p>You can paint it! ;D</p>
tristan on PRT-08631 - RCA Jacktristanurn:uuid:648b7572-40b0-31c1-d454-a395e6e0a1262010-05-09T17:54:22-06:00<p>It is in the SFE Eagle library, but only the footprint. The footprint is called "RCA". You need to make your own symbol and device.</p>
FazJaxton on PRT-08631 - RCA JackFazJaxtonurn:uuid:432f60c2-8ee1-cb78-bd9c-21278cc1dfa02010-02-04T20:32:16-07:00<p>Yeah, I couldn't find it in there either. :(</p>
davbeck on PRT-08631 - RCA Jackdavbeckurn:uuid:e28272bf-6446-e268-f888-14eb8198f81c2010-01-25T00:43:48-07:00<p>SparkFun needs to carry this in red and white!</p>
rahji on PRT-08631 - RCA Jackrahjiurn:uuid:24820515-cf5e-c95d-b25a-6bd4e009378f2009-09-01T16:26:39-06:00<p>Am I crazy or is this part not really in the SFE Eagle Library? Thanks for any info.</p>