SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-29T01:32:49-06:00SparkFun ElectronicsCustomer #514211 on COM-08642 - Reed SwitchCustomer #514211urn:uuid:98fbbda9-e1d4-7cb9-7f86-6cc03105fa032014-01-27T22:16:09-07:00<p>Thanks for the help!</p>
Customer #514211 on COM-08642 - Reed SwitchCustomer #514211urn:uuid:7f37f4f5-e16f-ee2d-34fc-0e7e3dafc95d2014-01-27T22:14:41-07:00<p>I want to turn a light on when a lid opens. Could I attach this to the wire, put a magnet on the lid, and have the lights off when the lid was closed?</p>
Customer #335103 on COM-08642 - Reed SwitchCustomer #335103urn:uuid:72c16423-54b9-1910-281a-bf55dea4c21e2014-01-20T21:01:50-07:00<p>ok, i will give them a shot.<p>i tried the hall effect sensors.</p><p>they worked but the latching is a problem. the reed switches seem like a simpler solution for what I am doing.</p></p>
Toni_K on COM-08642 - Reed SwitchToni_Kurn:uuid:525123cd-6799-28e1-d113-160b2b7218ef2013-12-27T09:16:14-07:00<p>This would work well for the application you are referring to. However, depending on what type of material you put over the piece, you may need an extremely strong magnet to trigger the reed switch. You may want to consider embedding the switch flush into each square so it can be more easily activated by the magnetic pieces.</p>
Customer #335103 on COM-08642 - Reed SwitchCustomer #335103urn:uuid:8de38d52-9ca9-a7f0-ef5c-3b3a3e2d1ebb2013-12-27T09:04:50-07:00<p>i am making a chess board that will automatically record moves (and eventually store in pgn format)
Will this type switch work for that application. I would mount the switch (64 of them, 8 x 8) under the board
then, using magnetic chess pieces, the switch would activate when a piece is moved.<p>I need something small and low cost. that can fit in the size of a chess square and work through a small piece of wood or cardboard. a $5 switch would make for an expensive project.</p></p>
Aurelio on COM-08642 - Reed SwitchAureliourn:uuid:19944d80-e975-b7db-822d-17f7b5a6bbf52013-08-19T12:26:38-06:00<p>Adding the on-time and off-time is not a suitable way to calculate resonant frequency. A switch in a resonant state is closing with both the magnetic force and the spring compression from the previous cycle, thus is accelerating slightly faster than a switch that was at rest before. When the switch is opening, it is also assisted by the spring compression from the previous cycle. I think that explains why resonant frequency is faster than merely adding on and off times. To illustrate by mechanical analogy: an SUV won't roll over if you swerve once, but if you swerve two or three times it might because each swerve builds up the potential energy on the springs as it bounces back and forth eventually building enough energy for the rollover. Of course, the closer the repeated swerves are to the roll mode resonant frequency of the suspension the greater the chances of roll over.</p>
The Doctor Doge on COM-08642 - Reed SwitchThe Doctor Dogeurn:uuid:fa5cf506-b981-6e78-6ca7-3de63bdcef9b2013-08-05T10:19:07-06:00<p>https://www.sparkfun.com/products/10601</p>
MikeGrusin on COM-08642 - Reed SwitchMikeGrusinurn:uuid:ea516aea-5966-728c-aa12-50b39d66961e2013-05-28T12:42:45-06:00<p>We're sorry about your poor experience. All reed switches are extremely fragile; if you need to bend the leads you MUST use a needle-nose pliers between the bend and the glass (but not touching the glass) to prevent ANY stress from being transmitted to the glass. Even better is not bending the leads at all. If you contact Customer Service (tell them I sent you) we'll see about getting you a replacement.</p>
Customer #125087 on COM-08642 - Reed SwitchCustomer #125087urn:uuid:f811da50-c6d1-5167-f617-6652c89427552013-05-28T11:56:40-06:00<p>Stay away! The glass broke on both the ones I bought with just the slightest bending of the pins. First thing I've bought from Sparkfun that I would qualify as junk.</p>
Customer #430748 on COM-08642 - Reed SwitchCustomer #430748urn:uuid:19d157c4-dc7b-4a93-2349-c4f6aff335332013-05-10T20:05:28-06:00<p>used this for a switch in my wall, LOVE neodenium.</p>
steven6282 on COM-08642 - Reed Switchsteven6282urn:uuid:fb06f9e7-8f7c-be26-fedd-91643eed51d32012-07-28T10:17:46-06:00<p>These reed switches are horrible. I highly recommend anyone looking for one to stay far far away from these. First problem, the tube is very very brittle. If you don't bend the pins very carefully it will break rendering the switch useless. Second problem, I don't know how or why but the switch itself is for some reason is holding a charge after the magnet is removed. Simple test with arduino, have an led set to turn on when a digital pin is low, feed power through the reed switch to that pin. Add a magnet the led turns off immediately, remove the magnet there is a 15 or 20 second delay before the led turns back on. Remove the reed switch and just touch the power wire to the pin wire together and led turns off and on immediately. I even tried just putting power to the leg of the switch on the same side as the arduino pin to make sure the switch wasn't getting stuck closed and it still had the delay when the power was removed. You can add a pull down resistor on the pin side to correct this, but it's annoying having to use up another component for it. These things aren't worth 15 cent each, must less the 1.50 price.</p>
Tareq on COM-08642 - Reed SwitchTarequrn:uuid:cc62cc80-afe1-4a03-b2ce-2fb8a0f7d0bb2012-07-24T16:07:29-06:00<p>Small 5.0 x 2.2 x 1.8mm Normally Closed (N/C) reed switch: <a href="http://www.meder.com/smd-sensors_mk24_uk3.html?&tx_jppageteaser_pi1%5BbackId%5D=2809" rel="nofollow">Here</a></p>
sfusco on COM-08642 - Reed Switchsfuscourn:uuid:e62ee7aa-48e7-c365-73c5-8501ab2789d62012-07-12T13:39:11-06:00<p>For those asking about normally closed: <a href="http://www.meder.com/magnet_actuation_us12.html" rel="nofollow">use two magnets</a></p>
Gather on COM-08642 - Reed SwitchGatherurn:uuid:c38117c1-198e-f770-01ff-d5d32f3147eb2012-04-23T15:17:51-06:00<p>where can i get a normally closed reed switch?</p>
baum on COM-08642 - Reed Switchbaumurn:uuid:7a46a790-7fe7-69f8-ba8c-7d7f9d90f1742012-03-18T10:23:58-06:00<p>Normally-Closed, please?<p>kthxbye.</p></p>
relaxing on COM-08642 - Reed Switchrelaxingurn:uuid:d3d75316-d7fd-daa8-2655-9629743471132012-01-08T09:23:34-07:00<p>Well let me be the first to say, no joke, these things are fragile. If you try to bend the leads while holding the glass barrel, the glass will snap.<p>Also the leads are steel, and will attract the magnetic half of the switch. Design accordingly.</p></p>
Customer #141410 on COM-08642 - Reed SwitchCustomer #141410urn:uuid:9f851322-ffe3-71e4-7f7e-c2b2389696092011-04-27T16:05:34-06:00<p>Go to the manufactures web site. You will learn more that you want. These switch's have very tight tolerances. When you look you will be amassed.</p>
tecker on COM-08642 - Reed Switchteckerurn:uuid:25bbd36e-0624-1928-21a6-b016624b3ae52011-03-26T22:55:23-06:00<p>When installing one of these is it important to pay attention to orientation? If I put 2 orthogonal (90deg) to each other could I put them near each other and not have the fields interfere with each other?</p>
williams on COM-08642 - Reed Switchwilliamsurn:uuid:f7907d87-494c-6140-a086-9c2de260f0fd2011-01-01T19:21:04-07:00<p>How many cycles can be expected on avg?</p>
RobertC. on COM-08642 - Reed SwitchRobertC.urn:uuid:2f528de4-9957-bf6d-a548-36d6c82146b92010-08-10T14:25:25-06:00<p>Or is your monitor just upside down? Just kidding. That's the only datasheet we got from them. Right click, rotate, it should work just fine.</p>
Kevin Vermeer on COM-08642 - Reed SwitchKevin Vermeerurn:uuid:c7a04155-02a0-fe4d-c72a-0325469e0fee2010-07-31T15:12:05-06:00<p>The datasheet is upside down.<br>
Tested in Preview on Mac OS X, Foxit PDF and Adobe Reader on Windows XP, and xpdf on Debian.<br>
Also, what it mean for this device to have a resonant frequency of 3.9kHz? That is significantly faster than the 1.25kHz frequency which would be indicated by the sum of the on-time (0.6ms) and off-time(0.2ms).</p>