SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T08:20:28-06:00SparkFun Electronicst00thPIK on COM-08643 - Magnet Square - 0.25"t00thPIKurn:uuid:eb27bf75-941a-974f-8599-9980309278332015-08-08T02:38:38-06:00<p>This might be a silly question, but I am a noob: Will this work well in a Hall Effect set up for a joystick? Or would a bigger/smaller/different shaped one be better?
Cheers</p>
Customer #590127 on COM-08643 - Magnet Square - 0.25"Customer #590127urn:uuid:9570e8a8-60fa-c33a-aab4-bd04efc5d2d82014-11-26T04:08:20-07:00<p>Hello, I'm from Philippines. Please have a re-stock of this product. We need 10pcs of this for our thesis.<p>Thank You!</p></p>
Customer #344545 on COM-08643 - Magnet Square - 0.25"Customer #344545urn:uuid:9cafa044-c31c-8fd1-8b43-7e7002fcb2852012-09-08T18:05:47-06:00<p>Also that they forgot to state the grade :)</p>
mkruse on COM-08643 - Magnet Square - 0.25"mkruseurn:uuid:74e65f1e-060f-44c9-ba87-980df4cf5a702012-02-25T14:40:20-07:00<p>Has anyone ever been in one of those moods? The kind that make you feel the need to point out that this is a cube, not a square?</p>
baum on COM-08643 - Magnet Square - 0.25"baumurn:uuid:43442a59-5e74-4d23-52e6-5e2c09e5c90d2011-04-24T17:03:16-06:00<p>No... not that. I'm trying to hack some devies with magnetic expansion ports on them, but I just realized I can solder directly on to the ports.</p>
Customer #30702 on COM-08643 - Magnet Square - 0.25"Customer #30702urn:uuid:12be30dc-9000-7213-673d-6fc5531bc3502011-04-01T04:47:55-06:00<p>Very strong magnets. Fun to play with.</p>
jma89 on COM-08643 - Magnet Square - 0.25"jma89urn:uuid:e6fe0115-4021-2cb5-2fe4-38273833ae122011-03-24T21:13:07-06:00<p>If you are going for an easy way to connect boards together you might wanna look at the magnet ring listed below.<br>
[Just came from there and they mentioned that very use in the description.]</p>
Customer #101672 on COM-08643 - Magnet Square - 0.25"Customer #101672urn:uuid:2a084578-d812-644c-d83f-996d3308899e2011-02-28T16:40:13-07:00<p>They are typically nickel plated, so yes, they are conductive, although I imagine it would be hard to solder to.</p>
baum on COM-08643 - Magnet Square - 0.25"baumurn:uuid:68abfb5f-da7e-cb13-437c-0616011cbef42011-02-24T14:47:15-07:00<p>Are these conductive? Can I solder a wire on to one?</p>
Datalink on COM-08643 - Magnet Square - 0.25"Datalinkurn:uuid:6679676b-0d4b-5c52-a7ee-6cd1755600f72011-01-07T08:29:44-07:00<p>Well, enough of them definitely could... though the weight rating isn't listed on the page, so we won't know until it is.</p>
jeffmcc on COM-08643 - Magnet Square - 0.25"jeffmccurn:uuid:53903455-c166-adfa-faa0-d8d155f73b9a2010-08-16T00:03:47-06:00<p>lrhol!</p>
I2C Master on COM-08643 - Magnet Square - 0.25"I2C Masterurn:uuid:9c9594b4-4a47-74fb-adfa-feaf4411f7402009-11-20T20:50:46-07:00<p>Is the "hold small children" part true!</p>