SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T15:20:44-06:00SparkFun ElectronicsAgustinGS on WRL-08771 - Bluetooth SMD Module - BluegigaAgustinGSurn:uuid:12338c76-a523-93cd-907d-ac47f4f894432013-03-29T12:48:58-06:00<p>Hi guys,<p>"The module can be configured to operate autonomously", does this mean I can set it up with my project without the need of a microcontroller/arduino? and send the signal directly to a smartphone? that'd be awesome...</p><p>thanks</p></p>
FD on WRL-08771 - Bluetooth SMD Module - BluegigaFDurn:uuid:5b085876-e294-78de-a609-839e6d6c016b2013-01-31T21:14:29-07:00<p>We found this great Bluegiga WT12 USB dongle here http://esdn.com.au/store.htm I heard it is also available on inmojo.com</p>
Customer #402069 on WRL-08771 - Bluetooth SMD Module - BluegigaCustomer #402069urn:uuid:a9da367f-a79d-2113-6ed9-409f239ecc162013-01-25T08:11:44-07:00<p>Hello...
Currently i'm trying to do a pet detector using Bluetooth so may i know which Bluetooth module that is able to measure the range distance?
Hope for advice asap,thx^^</p>
Toni_K on WRL-08771 - Bluetooth SMD Module - BluegigaToni_Kurn:uuid:f30f2b6a-ce97-5d40-d55c-eae58bdf614e2012-10-03T13:08:49-06:00<p>Unfortunately we did, as it was too slow of a seller. However, you can find it on a breakout board <a href="https://www.sparkfun.com/products/8952" rel="nofollow">here</a>.</p>
FlippinJax on WRL-08771 - Bluetooth SMD Module - BluegigaFlippinJaxurn:uuid:a3bf1331-9538-4cfd-b246-d886c384d8302012-09-26T21:32:15-06:00<p>Did you guys stop carrying this?</p>
Customer #316403 on WRL-08771 - Bluetooth SMD Module - BluegigaCustomer #316403urn:uuid:02834a8c-50d7-9755-088e-088ead7794df2012-04-25T14:12:36-06:00<p>Does anyone know which bluetooth is connectable to Android?</p>
GearJammer on WRL-08771 - Bluetooth SMD Module - BluegigaGearJammerurn:uuid:234594b5-ce98-bf05-44be-f289f1136c892012-01-24T20:11:31-07:00<p>It's made to charge a 1 cell Lithium poly battery. 4.2V is the max voltage you want a 1 cell to reach as you're charging it. 3.7V is the nominal voltage of the cell. Fully charged it will sit at 4.2V. Once you start pulling current from it the voltage will sag to 4.1V down to 3.1ish then it's dead and needs to be recharged. So yes it's suitable.</p>
LeX_Luther on WRL-08771 - Bluetooth SMD Module - BluegigaLeX_Lutherurn:uuid:8aa7f30a-702f-f970-a7e4-51096c6cc0b52011-08-15T21:50:22-06:00<p>It is suitable for the 3.7V Lithium Polymer Battery the charge cut off voltage is 4.2</p>
Bunk on WRL-08771 - Bluetooth SMD Module - BluegigaBunkurn:uuid:882a6647-9d9c-a87c-3f8b-71f44fb7a5142011-04-12T09:19:59-06:00<p>Will the battery charger on this be suitable for a 3.7V Lithium? It says it charges at 4.2V</p>
ARTTEC on WRL-08771 - Bluetooth SMD Module - BluegigaARTTECurn:uuid:ba2caadd-ea0b-6091-54b5-b6b225d8c6342010-09-20T17:25:12-06:00<p>I have a project where I need to send analog audio and transmit it to something like a (generic??) bluetooth cell phone earbud. Anyone know whether this module can do that?</p>
Agentx on WRL-08771 - Bluetooth SMD Module - BluegigaAgentxurn:uuid:dcc9d2c1-6fc3-d3d4-843a-dc5b2a8c9c8f2010-09-09T21:51:10-06:00<p>I need a bluetooth hub. I have 3 bluetooth stereo speakers but can only connect to 1 from my current bluetooth usb adapter on my computer. Is there anything like a bluetooth hub where I can connect all 3? Your suggestions are warmly welcome.<br>
Thanks</p>
sirius506 on WRL-08771 - Bluetooth SMD Module - Bluegigasirius506urn:uuid:8bdbf92e-6deb-b7d3-8f71-38944ed4dc7b2010-07-03T21:13:38-06:00<p>Bluegiga offers DFU tool with new firmware and it allows you to upgrade through serial port. You don't need to use SPI. I have successfully upgraded my breakout board comes with iWRAP3.0 to iWRAP4.0 through serial port.</p>
sqnewton on WRL-08771 - Bluetooth SMD Module - Bluegigasqnewtonurn:uuid:240a50dc-8ac0-b2f7-1f17-73646a29e48f2010-06-17T11:35:31-06:00<p>BlueGiga released a couple of months ago the iWRAP4 FW. Do your WT32 have iWRAP4 or 3 loaded? If v.3, do you plan to upgrade them to 4, or ask BlueGiga for an upgrade? For us (users) the upgrade is sort of a pain, since requires an extinct PC parallel port, external circuitry and access to SPI pins. Thx!</p>
reginr on WRL-08771 - Bluetooth SMD Module - Bluegigareginrurn:uuid:f22f3160-9751-c0ea-3b0d-bf3948246e6d2010-04-19T03:14:07-06:00<p>what is the iWrap firmware version on this chip? Please advise,<br>
Thanks</p>