SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-29T05:35:08-06:00SparkFun ElectronicsWolfram on COM-08862 - Super Bright LED - Red 10mmWolframurn:uuid:e345a62a-6a83-a0fa-f6de-603502fff72b2013-10-22T19:29:34-06:00<p>These LEDs are aptly named! (You'll probably need some sort of diffuser.)</p>
Thesmug on COM-08862 - Super Bright LED - Red 10mmThesmugurn:uuid:c2bdad89-9468-2da7-e46a-9db1e0320e1a2013-04-17T21:01:29-06:00<p>Anybody else order these and get UV leds instead?</p>
Scottm on COM-08862 - Super Bright LED - Red 10mmScottmurn:uuid:a270fe0d-a2aa-1542-ff91-114fafb3f5242012-06-07T22:47:16-06:00<p>I've made more of these flashlights and instead of using diodes I have switched to a 6.8 ohm resistor. This pulls about 87 mA on a full 3V which seems to be about right for a 2 AA cell flashlight.</p>
kg2li on COM-08862 - Super Bright LED - Red 10mmkg2liurn:uuid:fcc4a1dc-c3f9-de36-2dbd-f6ae8ec7f5942012-01-30T18:53:15-07:00<p>I added a few of the green 10mm Super Brights to my last order just for fun, Sparkfun # COM-08861. Just 5 mA was enough to make the green ones hurt your eyes; 40 mA lit up the room. I would imagine that these red ones are just as impressive.</p>
NewsparkFunCusty on COM-08862 - Super Bright LED - Red 10mmNewsparkFunCustyurn:uuid:161b4082-2655-9b1d-de7c-97bd05f28b1a2011-03-09T12:24:38-07:00<p>any chance of 25 packs of these?</p>
Scottm on COM-08862 - Super Bright LED - Red 10mmScottmurn:uuid:214e3145-2e95-4b70-bdfb-7fdfc68548d62010-02-05T23:36:01-07:00<p>Wow I loved this LED. I put it into a one dollar flashlight <em>along with two extra diodes to drop voltage</em> and Wah-La! I have a very powerful red flashlight for under three bucks!</p>