SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-19T03:53:46-06:00SparkFun Electronicsjcraig111 on TOL-08981 - Switching Power Supply - 24V 500mAjcraig111urn:uuid:acfdd8ab-f891-a8be-16d1-eccd9c188eb92011-04-20T20:59:07-06:00<p>OK for all of you that are still wondering about the "+ /- " question. You will get +24 between the - and + out puts. Measuring either one to the common ground will give you nothing. The ground is for the AC in. I got one of these and tested it so this is what I found. Hope that is helpful.</p>
WillWD on TOL-08981 - Switching Power Supply - 24V 500mAWillWDurn:uuid:9ea1a853-98c9-be4b-36fa-2af1a3fb7a712011-01-04T05:18:10-07:00<p>Hi, It takes it from AC +/- and makes it 24VDC +/- with the FG as a ground, eg. house... I think.. does this help?</p>
John_CA on TOL-08981 - Switching Power Supply - 24V 500mAJohn_CAurn:uuid:c687d5b5-fbe2-dead-9720-9885ed2a7bfb2010-01-30T17:36:03-07:00<p>I would like to echo the "stupid question". Is "FG" 12 or 24 volts from the +/- pins? i.e. Do you get 48 volts from +V to -V or do you get 24V?</p>
tomcuga on TOL-08981 - Switching Power Supply - 24V 500mAtomcugaurn:uuid:19f70efe-453e-efcd-7d87-bbedc2a221d82009-10-22T06:02:57-06:00<p>what is trimmer used for?</p>
GETSEMAN on TOL-08981 - Switching Power Supply - 24V 500mAGETSEMANurn:uuid:acfc6a00-ef19-45a0-ea6e-04c07d45b2352009-09-08T08:59:06-06:00<p>Any one has an idea if this 24V 500mA PS suitable to drive directly a string 6 or 7 power leds (e.g. Lumiled star LXHLMWId 3.42V 350mA)?.</p>
JRiggles on TOL-08981 - Switching Power Supply - 24V 500mAJRigglesurn:uuid:f1c827e0-efa7-3146-13d3-be415238e7442009-04-07T20:44:16-06:00<p>(possibly stupid question) I'd like to run this as a dual polarity supply: is it safe to assume that this will give me +/- 24v at the DC output(s)? Or will I get +24v total and I'll have to split-rail it for +/- 12v DC?</p>
Rubi on TOL-08981 - Switching Power Supply - 24V 500mARubiurn:uuid:12dff88d-d5d1-772a-9795-22329175c4bf2009-02-12T02:33:10-07:00<p>Hi<br>
I was lucky and could snatch one of these, but they were sold out on the first day. I hope you will restock them.<br>
Cheers<br>
Rubi</p>