SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T11:34:06-06:00SparkFun ElectronicsCustomer #1504424 on TOL-09146 - SparkFun Mini ScrewdriverCustomer #1504424urn:uuid:b030a4d2-086c-cb1c-5c53-8667d7a5651e2019-02-24T23:43:18-07:00<p>a useful <a href="https://www.culturism.net/concentrate-proteice/optimum-nutrition-100-whey-gold-standard-2-3-kg.html" rel="nofollow"></a> thing</p>
Lawrence K. on TOL-09146 - SparkFun Mini ScrewdriverLawrence K.urn:uuid:3d27f8a1-4be4-55a6-7ee6-093c47ff98af2014-01-07T19:28:04-07:00<p>I just received four of these. Two of them won't stay in the socket and fall right out. The other two are slightly snug, but slide out when shaken. I recommend not buying.</p>
Funda on TOL-09146 - SparkFun Mini ScrewdriverFundaurn:uuid:8cddc8ba-f2c4-5b4b-81c0-74cb62bf618a2013-03-29T14:48:54-06:00<p>No, the screw bit should fit very snug inside the socket. Contact tech support if you are still having issues(techsupport@sparkfun.com)</p>
Brandon P on TOL-09146 - SparkFun Mini ScrewdriverBrandon Purn:uuid:b8fa89ba-95a0-8dcd-ce09-327630050bd62013-02-18T15:37:59-07:00<p>I just received mine today. Is the screw bit suppose to be so loose in the socket? I can't imagine keeping this clipped in a pocket or pocket protector without worrying about losing the bit.</p>
Customer #327198 on TOL-09146 - SparkFun Mini ScrewdriverCustomer #327198urn:uuid:d2feb3f1-afc5-9de0-a39a-e582ac5c4ea52012-08-23T22:18:09-06:00<p>Awesome sqew driver get it with your order</p>
SomeGuy123 on TOL-09146 - SparkFun Mini ScrewdriverSomeGuy123urn:uuid:8104311d-166c-034a-97fb-1315c7386d9f2011-07-02T07:59:10-06:00<p>It's easy to grind it down a bit though. Sparkfun should consider carrying plastic screwdrivers. Those are useful for adjusting trimpots without shorting them out.</p>
pcmofo on TOL-09146 - SparkFun Mini Screwdriverpcmofourn:uuid:87344c5a-f98e-1eb0-6a6d-383724ec13f92009-10-06T19:09:06-06:00<p>I thought this would work great for tweaking small POT's and screw terminals. It's just slightly too big to do either :-/</p>