SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T15:09:18-06:00SparkFun ElectronicsToni_K on SWG-09192 - SparkFun Coffee MugToni_Kurn:uuid:27df5d65-429a-dc07-4382-342926f60c4a2013-10-09T09:16:20-06:00<p>I <em>think</em> they got pulled off store front so we can use them as swag for events like Maker Faires and class workshops, as well as caption contests and the like.</p>
djfunk on SWG-09192 - SparkFun Coffee Mugdjfunkurn:uuid:8e0f34ab-1fd6-a71a-5963-4168890f2b422013-10-08T19:19:32-06:00<p>RETIRED?! I was just about to add it to my cart... (Any spares?)</p>
Customer #401698 on SWG-09192 - SparkFun Coffee MugCustomer #401698urn:uuid:2f76cc5a-f606-0949-4271-19926f7f10b22013-06-21T16:37:41-06:00<p>Most would think geek is an insult but it can be taken as a compliment too.
I'm not afraid to admit I'm a geek.</p>
icyfyer on SWG-09192 - SparkFun Coffee Mugicyfyerurn:uuid:af56cddf-7d15-82af-8705-1af46b8106b72012-08-15T09:19:08-06:00<p>Don't buy it.</p>
Customer #167681 on SWG-09192 - SparkFun Coffee MugCustomer #167681urn:uuid:da66e575-dcf3-596f-7b43-ee365d7d255a2012-03-05T13:32:29-07:00<p>Just got my cup. When held in the left hand the logo faces outwards. Since I'm a left hander it is awesome!</p>
jrossetti on SWG-09192 - SparkFun Coffee Mugjrossettiurn:uuid:b63f3a3a-4969-7ef6-00dd-e4d285d157c12011-06-28T07:22:42-06:00<p>This mug is awesome. 8 oz of liquid fills the mug to more-or-less the exact point where the 'hook' on the inside of the handle stops. This allows for perfect in-mug measuring of your favorite instant beverages!<br>
The extended capacity is also a welcome bonus if you're drinking liquids other than instant powdered stuff - it's a perfect vessel to disguise my beer and avoid the condescension of my beer-hating wife.</p>
pressurepoint14@gmail.com on SWG-09192 - SparkFun Coffee Mugpressurepoint14@gmail.comurn:uuid:68ef6cc6-5b6c-cbac-13ea-bc37cd6ce5fc2011-02-25T22:36:30-07:00<p>and that's why it says geek</p>
N.Poole on SWG-09192 - SparkFun Coffee MugN.Pooleurn:uuid:ed81cb9d-91b3-6e92-2235-29b674f467062011-02-21T13:18:25-07:00<p>I've owned this product for a few weeks now. It shows an incredible compatibility with most beverages, it seems to have positively effected my geek-rating, and is totally RoHS compliant (no dangerous levels of lead in my coffee)...<br>
I did have to add cream and sugar for my application, so it'd be nice to see a break-out board with those components integrated. Great part, though, and I may buy some more (you know, so I can network them.)<br>
;)</p>
N.Poole on SWG-09192 - SparkFun Coffee MugN.Pooleurn:uuid:8a397e63-13e7-7f02-bcf4-06a1bf001af92011-01-15T11:14:29-07:00<p>I'm a geek... I'll admit it.<br>
But it's all good, geeks are cool now.<br>
Reference the Venn diagram in RogueBoticist's post:<br>
Obsessive and Intelligent but NOT socially inept.<br>
I'm also a coffee geek... And I need more mugs...<br>
I do have all that FreeDay Cash...</p>
Rogue on SWG-09192 - SparkFun Coffee MugRogueurn:uuid:1a3dd53b-6539-ac81-6eb1-140b7c1b2f8a2010-06-08T16:09:02-06:00<p>Nerd could be considered a step up to some... see this awesome Venn diagram!:<br>
<a href="http://i192.photobucket.com/albums/z167/Great_WhiteSnark/Nerd_Dork_Geek_Venn_Diagram.jpg" rel="nofollow">http://i192.photobucket.com/albums/z167/Great_WhiteSnark/Nerd_Dork_Geek_Venn_Diagram.jpg</a></p>
Finnishguy on SWG-09192 - SparkFun Coffee MugFinnishguyurn:uuid:a7adc7b2-9241-2bf0-585c-ad6f48c5aba42010-05-18T05:49:11-06:00<p><strong><a href="account.php?id=6862" rel="nofollow">billiam2536</a>:</strong> <em>"something we use everyday, like ohms law." Geek.</em><br>
Hah :) But at least it doesn't say it directly. Maybe I should step out from closet :D</p>
billiam2536 on SWG-09192 - SparkFun Coffee Mugbilliam2536urn:uuid:51bed091-690c-d655-378a-45898a1a92b32010-05-14T22:15:59-06:00<p>"something we use everyday, like ohms law." Geek.<br>
might have to buy it anyway. I love mugs.</p>
Finnishguy on SWG-09192 - SparkFun Coffee MugFinnishguyurn:uuid:7dfd8c36-bb98-77d1-244f-2355c2d8ed672010-05-02T12:12:53-06:00<p>Or picture of Atmega 328? Or some well known schematics, for example basic 7805-circuit (capacitors etc). Or some electronic formulas that we use every day, ohm's law.. Anything. Not "geek". I'm not a geek.</p>
Finnishguy on SWG-09192 - SparkFun Coffee MugFinnishguyurn:uuid:b05bc367-edb0-fff5-c3f8-a4f5971b7c482010-02-26T04:45:35-07:00<p>Why it has to say "Geek"? I don't feel that word "geek" is a word that I want to be on my coffee mug.<br>
Better ideas "DIY" or "RTFM" ..</p>