SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-29T05:41:48-06:00SparkFun ElectronicsCustomer #502493 on COM-09414 - Microswitch - 2 TerminalCustomer #502493urn:uuid:5071f0f3-c64a-0567-a9ac-c9fbdd185f412014-01-26T01:08:21-07:00<p>Does anyone know the size of the mounting holes?</p>
Customer #255632 on COM-09414 - Microswitch - 2 TerminalCustomer #255632urn:uuid:3251bbb6-c0c7-418d-74f4-d3e9fb32200e2013-02-08T01:17:32-07:00<p>Yes</p>
Sofia on COM-09414 - Microswitch - 2 TerminalSofiaurn:uuid:032ada66-db6f-13c2-01f0-b15a9bca529a2012-08-19T07:17:47-06:00<p>Can we get a data sheet fo rthis please.</p>
rlankenau on COM-09414 - Microswitch - 2 Terminalrlankenauurn:uuid:5eea35f0-7cd6-e3ac-04d0-3be1e15860f52012-02-12T10:27:16-07:00<p>Can anyone recommend a connector to use on these switches? Or, lacking a solid recommendation, what are the dimensions of the leads?</p>
ThinkerT on COM-09414 - Microswitch - 2 TerminalThinkerTurn:uuid:3d1a3caf-53e9-c68f-ea44-6827d8ded41d2012-01-13T19:00:28-07:00<p>Thanks for your comment! That's what I was planning to use them for! Are they effective?</p>
scrappy64 on COM-09414 - Microswitch - 2 Terminalscrappy64urn:uuid:a6d36355-4bef-2b7c-568b-9705a71f3d4f2011-10-05T21:31:11-06:00<p>Anyone have any comments about weather resistance of switch in an outside application? Appears to be pretty well sealed with the exception being the openings to prevent range of motion of the moving parts.</p>
laserhawk64 on COM-09414 - Microswitch - 2 Terminallaserhawk64urn:uuid:fa93b41d-42e7-9227-9da5-e1918500170c2011-09-29T00:38:49-06:00<p>It looks to be similar to the three-terminal version, here:<br>
http://www.bao-lian.com/en/?p=3489<br>
I've uploaded their dimensional drawing of that switch to Imageshack (to avoid leeching), here:<br>
http://img88.imageshack.us/img88/5711/10318000n.jpg<br>
I hope that this proves useful.</p>
SomeGuy123 on COM-09414 - Microswitch - 2 TerminalSomeGuy123urn:uuid:ded810a7-cc4f-ccd5-2d7b-0c3d259c77682011-07-23T05:50:36-06:00<p>It <a href="http://dlnmh9ip6v2uc.cloudfront.net/images/products/09414-1.jpg" rel="nofollow">looks like</a> they are normally open.</p>
WizenedEE on COM-09414 - Microswitch - 2 TerminalWizenedEEurn:uuid:b42f6f6e-5a3c-19c3-51f8-fccc4dcc8a442011-07-22T00:36:48-06:00<p>NO</p>
MisterFuzzy on COM-09414 - Microswitch - 2 TerminalMisterFuzzyurn:uuid:fe9742f0-8dbd-c9c8-a73e-fb4eebae84d22011-05-27T22:53:20-06:00<p>What's its thickness?</p>
vputz on COM-09414 - Microswitch - 2 Terminalvputzurn:uuid:b7671917-65aa-a6d8-8f5f-e15b5bc6d8402011-03-08T13:21:28-07:00<p>DeadTom (or others coming here later...)<br>
I bought a few of these for CNC limit switches not realizing that limit switches are normally NC rather than NO (which these are).<br>
However, these are easy to pry apart with a fingernail and small screwdriver; there is actually a small tab connected to the NC position, so these are really three-terminal microswitches but the NC terminal is essentially clipped flush with the case. I swapped the two terminals (the small metal tabs easily slide out of the case)and so far it seems to be working fine as an NC switch now.</p>
DeadTom on COM-09414 - Microswitch - 2 TerminalDeadTomurn:uuid:e8a2f25c-bd74-ca33-21a2-d7cf3da68c762010-12-27T09:04:38-07:00<p>Oops, sorry should have looked at the pics....</p>
DeadTom on COM-09414 - Microswitch - 2 TerminalDeadTomurn:uuid:c562e8ed-9a6e-8cf1-8def-0f09c91d514d2010-12-27T08:43:58-07:00<p>Is this a normally open switch or normally closed?</p>
Sam Lanzo on COM-09414 - Microswitch - 2 TerminalSam Lanzourn:uuid:95f78026-caad-5f28-dfa7-1de8333bbab92010-03-29T19:27:21-06:00<p>deleted</p>
wayland on COM-09414 - Microswitch - 2 Terminalwaylandurn:uuid:172dcce6-633d-0c3c-0cf1-cdd8ad3eb35b2010-03-01T01:03:11-07:00<p>is this momentary?</p>
wassabi on COM-09414 - Microswitch - 2 Terminalwassabiurn:uuid:556ce47b-056b-a59c-b593-6f149f2972622010-02-14T10:07:46-07:00<p>Wasn't blue, but worked great otherwise. Lever is great for all sorts of applications.</p>