SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-29T06:44:08-06:00SparkFun ElectronicsCustomer #469276 on BOB-09540 - SparkFun Full-Bridge Motor Driver Breakout - L298NCustomer #469276urn:uuid:8ed48ef4-1f14-7834-4912-c83886ebf66b2014-11-15T11:16:39-07:00<p>how can i calculate a current sensing resistor, and is it mandatory ?</p>
Customer #373632 on BOB-09540 - SparkFun Full-Bridge Motor Driver Breakout - L298NCustomer #373632urn:uuid:a8cc87f6-2350-dde2-70a4-fde752be7a772012-12-22T14:32:25-07:00<p>It work with Brushless motor?</p>
rocketman221 on BOB-09540 - SparkFun Full-Bridge Motor Driver Breakout - L298Nrocketman221urn:uuid:6cfd89a1-6b81-1462-8b11-3bd424f5c8b02012-02-11T16:41:08-07:00<p>Probably for someone using a text browser like w3m or lynx.</p>
fdjuri on BOB-09540 - SparkFun Full-Bridge Motor Driver Breakout - L298Nfdjuriurn:uuid:39a31839-cdf0-b464-708b-38c7c42746b72011-05-01T12:15:42-06:00<p>Why is there a link on a <strong>ASCII</strong> image of the board? For those who can't find it, it's just below the 4th image.</p>
RobertEly on BOB-09540 - SparkFun Full-Bridge Motor Driver Breakout - L298NRobertElyurn:uuid:ea3db81a-9089-86c8-53b9-ad7729ce93472011-03-22T21:04:06-06:00<p>Yes, you do.</p>
dezguy on BOB-09540 - SparkFun Full-Bridge Motor Driver Breakout - L298Ndezguyurn:uuid:930d7e65-f4bc-af31-2f64-73ecae156a242011-02-21T10:26:56-07:00<p>Do you need to use schotky diodes on this still? All of the circuits I've seen with this chip do?</p>
stilldavid on BOB-09540 - SparkFun Full-Bridge Motor Driver Breakout - L298Nstilldavidurn:uuid:664e84d8-1aec-cb40-00f7-2dcf656e0db32011-01-31T16:59:24-07:00<p>Just one. Generally you'll you put the IC in, flip it over and just solder on the bottom side of the board (the side with the sparkfun logo on it). The <a href="http://en.wikipedia.org/wiki/Via_(electronics)" rel="nofollow">vias</a> go all the way through the board.</p>
Customer #188362 on BOB-09540 - SparkFun Full-Bridge Motor Driver Breakout - L298NCustomer #188362urn:uuid:afdfac04-026e-53d4-ffb3-84b769709e572011-01-31T15:09:05-07:00<p>This board is double sided. Does that mean that I have to solder both sides or just one?<br>
Regards<br>
Allan</p>
Rogue on BOB-09540 - SparkFun Full-Bridge Motor Driver Breakout - L298NRogueurn:uuid:4a915b4e-ec10-873d-7e04-dd4cc26143a82010-05-28T16:21:28-06:00<p>Just want to note that you can slightly bend the leads using pliers to fit a .1" pitch breadboard across its center line.</p>