SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-29T08:59:11-06:00SparkFun ElectronicsJustinS. on PRT-09572 - Binding Post Pair (Black/Red)JustinS.urn:uuid:df6a419a-febb-e4f4-0c1c-df0a0f59937d2011-03-22T22:32:12-06:00<p>They Have an insulating base for installation into sheet metal.</p>
JustinS. on PRT-09572 - Binding Post Pair (Black/Red)JustinS.urn:uuid:0d94034c-b308-f133-8faf-9a43991af9542011-03-22T22:30:49-06:00<p>None,<br>
The end is solid. To use this you need to either install ring terminals on your wires, or wrap the wire around the post.</p>
JustinS. on PRT-09572 - Binding Post Pair (Black/Red)JustinS.urn:uuid:6a0cb0a1-3d83-ce1e-3360-059b504b83d42010-01-12T11:32:35-07:00<p>I received some of these through free day, Only received the black ones not a pair but I cannot complain with free day. A few notes on these<br>
1. These seem to be bigger than most common binding posts, but I would bet that is because they are for high current applications<br>
2. No banana jack , which was stated, however they also do not have the cross drilled hole for a wire to stick through. So you will either need to wrap your wire around the post, or use a ring terminal to connect to it.<br>
3. The mounting is somewhat insulated. It should work fine on sheet metal, up to maybe 1/16" thickness and even beyond that If you are careful in your mounting.<br>
4. The stud appears to be a 3/16" size you could most likely base your current capacity from this.<br>
5. The clear part is actually two pieces that separate to sandwich the mounting surface between them.<br>
6. The knob can be screwed completely off.<br>
Thanks Sparkfun!!!</p>
Hyratel on PRT-09572 - Binding Post Pair (Black/Red)Hyratelurn:uuid:e48bd7f3-9c82-5fc1-0b1d-f08596f224e72010-01-11T18:43:28-07:00<p>Voltage/amperage rating of these units? also, I cannot tell whether these are just insulated knob or if they have an insulated base (which would be needed for installing in a metal sheet)</p>
blen2r on PRT-09572 - Binding Post Pair (Black/Red)blen2rurn:uuid:6d776373-9118-453a-68a5-a5bd9b6e28632010-01-11T14:38:06-07:00<p>Hi,<br>
what kind of plugs fit in this if banana plugs don't?<br>
thank you</p>