SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T11:38:27-06:00SparkFun Electronicspp.kettu on LCD-09584 - Serial TFT LCD 3.2" with Touchscreenpp.kettuurn:uuid:143f7330-cef8-f60c-c646-5542000a32862009-12-24T16:19:07-07:00<p>Ok, not exactly low-cost. But it isn't just a display with touch screen, it's more with programmable processor, uSD card adapter, audio, GPIO...<br>
I don't know. It's hardly a bargain, but I guess there is also worse deals out there.</p>
Bradley on LCD-09584 - Serial TFT LCD 3.2" with TouchscreenBradleyurn:uuid:5e88eb70-6c8a-3cc4-2166-3e629e905ca32009-12-20T12:49:04-07:00<p>I have to agree as well. However, it really isn't Sparkfun's fault on the price. If you go to 4D Systems the price would probably be the same or higher. If 4D systems really want to sell displays at a price like this the It needs to be able to do a lot of stuff such as displaying webpages in HTML for example. I really don't see the point in 4D Systems selling a low resolution screen for this price especially when the display is slooooooooooooooooow. I have the uOLED-32024-P1 and I'm sending commands at 115200 with a picmicro which allowed me to get the display to speed up reponse in displaying circles, text and rectangles.</p>
Robban on LCD-09584 - Serial TFT LCD 3.2" with TouchscreenRobbanurn:uuid:fbf8678a-f7db-bd87-7919-49defacd1a802009-12-18T14:58:29-07:00<p>I think I have to side with frank26080115 here. $175 isn't exactly what I'd call "low-cost". For another 4 bucks one could buy an iPod Touch for example.</p>
frank26080115 on LCD-09584 - Serial TFT LCD 3.2" with Touchscreenfrank26080115urn:uuid:00999323-f7a1-7c6d-7ecf-d1c98f25c2142009-12-17T08:53:15-07:00<p>why do you guys insist on stocking super expensive products like this? that serial command set doesn't seem like such a huge advantage, and it'll be slooooow<br>
please stock some decent LCDs<br>
maybe like <a href="http://www.thaieasyelec.net/index.php/arduino/3-2-inch-tft-touch-screen-with-arduino-interface/p_68.html" rel="nofollow">http://www.thaieasyelec.net/index.php/arduino/3-2-inch-tft-touch-screen-with-arduino-interface/p_68.html</a> for $55</p>