SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T11:01:36-06:00SparkFun ElectronicsSlugEngineer on COM-09649 - DC Brushless Fan - 80x80x15mm (5V)SlugEngineerurn:uuid:568ed111-a134-5fd7-8fdc-b707c9e0b1cd2014-06-14T18:58:28-06:00<p>If I ran this at 6v how long til it would fail if at all?</p>
Kevin_S on COM-09649 - DC Brushless Fan - 80x80x15mm (5V)Kevin_Surn:uuid:2e4e2f3b-cf62-961c-2ed1-792d72f1ac1e2014-02-11T16:17:03-07:00<p>could this fan be used as a wind generator to power an Arduino pro mini and a standard servo using the wind of a leaf blower?</p>
Customer #302799 on COM-09649 - DC Brushless Fan - 80x80x15mm (5V)Customer #302799urn:uuid:4ab9d908-1803-3326-a5d0-ee63b715584f2013-06-05T14:52:40-06:00<p>360ma, you would be fine running it off of the 5v pin and ground, just don't try to run it off of one of the regular I/O (input/output) pins.</p>
Customer #302799 on COM-09649 - DC Brushless Fan - 80x80x15mm (5V)Customer #302799urn:uuid:75de1be8-3a8c-88a0-ef43-aed9341b7aa32013-06-05T14:50:04-06:00<p>Probably just regular 110v out of the wall that's been regulated to DC. Although that would have to be a pretty beefy circuit...</p>
Customer #74037 on COM-09649 - DC Brushless Fan - 80x80x15mm (5V)Customer #74037urn:uuid:29c347ba-ef5c-ca69-8941-0c2c47f76b0f2012-11-09T19:01:05-07:00<p>Can you run this fan from the a wall outlet powered arduino?</p>
RobertC. on COM-09649 - DC Brushless Fan - 80x80x15mm (5V)RobertC.urn:uuid:7408147d-5ef9-4b0c-df29-c01e4aae10332012-06-27T11:09:13-06:00<p>Sorry, but they sent the wrong thing and we're working on getting them re-shipped.</p>
Customer #273151 on COM-09649 - DC Brushless Fan - 80x80x15mm (5V)Customer #273151urn:uuid:c1b4a054-b182-5212-c0ee-b15fe5fb646a2012-06-26T18:18:56-06:00<p>When will these be coming in? Its been almost 2 weeks. :(</p>
StayPutNik on COM-09649 - DC Brushless Fan - 80x80x15mm (5V)StayPutNikurn:uuid:35193af8-d31b-6fdc-a9ec-89843722d1982011-08-31T10:03:46-06:00<p>do you need a brushless motor ESC to use one of these? or can you just hook it up to 5VDC?</p>
nojo on COM-09649 - DC Brushless Fan - 80x80x15mm (5V)nojourn:uuid:1d3c0f9d-d4ea-db16-f070-c27e37d2d7522011-04-10T02:35:36-06:00<p>:( more numbers</p>
SomeGuy123 on COM-09649 - DC Brushless Fan - 80x80x15mm (5V)SomeGuy123urn:uuid:4571a6a2-12ad-c3ea-0e17-5c2f9f9620922011-02-24T18:42:47-07:00<p>That depends on the humidity, temperature, and pressure the air in location that you are cooling.</p>
SomeGuy123 on COM-09649 - DC Brushless Fan - 80x80x15mm (5V)SomeGuy123urn:uuid:2e257f3b-7414-d4d3-2117-415f68fafa742011-02-24T18:40:55-07:00<p>Where did you find a 100v DC power source?</p>
SomeGuy123 on COM-09649 - DC Brushless Fan - 80x80x15mm (5V)SomeGuy123urn:uuid:caed8cf9-4d51-f334-523e-89e9149a4d0d2011-02-24T18:39:52-07:00<p>I believe the <code>B</code> in the product number means ball bearing. I could be wrong though.</p>
SomeGuy123 on COM-09649 - DC Brushless Fan - 80x80x15mm (5V)SomeGuy123urn:uuid:dbe56fc2-f76c-f27e-899e-fc2be02ce58d2011-02-24T18:38:47-07:00<p>According to the datasheet, 20.17CFM.</p>
nojo on COM-09649 - DC Brushless Fan - 80x80x15mm (5V)nojourn:uuid:05089f04-0a3d-ec6c-818a-28b5846d876b2011-01-27T22:04:44-07:00<p>:D datasheet dont help me any...<br>
does anyone know the max heat dissapation??</p>
doinky72 on COM-09649 - DC Brushless Fan - 80x80x15mm (5V)doinky72urn:uuid:58cf7b5a-2f0f-aaba-c17b-38c4fe1f92452010-12-05T20:00:01-07:00<p>What would it take to step 110 down to run this. I don't see any DC to DC converters that step down that type of voltage?</p>
PresidentOfAwesomeness on COM-09649 - DC Brushless Fan - 80x80x15mm (5V)PresidentOfAwesomenessurn:uuid:b4f00390-fba4-da2c-f247-fddc3d86c9332010-03-06T09:21:20-07:00<p>That's a link to a japanese clothes store. Thanks for the info though.</p>
Forrest on COM-09649 - DC Brushless Fan - 80x80x15mm (5V)Forresturn:uuid:29860221-0d3a-504b-8472-2b91343838b32010-02-26T00:47:58-07:00<p>From <a href="http://www.shvt.cn/en/uploaded_files/1256804264.pdf" rel="nofollow">http://www.shvt.cn/en/uploaded_files/1256804264.pdf</a><br>
2500 rpm, 29.17 CFM, .11 in-h20 static pressure, 28 dB-A noise, 54 g mass</p>
WimL on COM-09649 - DC Brushless Fan - 80x80x15mm (5V)WimLurn:uuid:20183a5f-4a67-a540-ee82-2de8631d28282010-02-21T13:31:57-07:00<p>It looks like this might be the manufacturer's page: <a href="http://www.shvt.cn/en/DC-FAN/" rel="nofollow">http://www.shvt.cn/en/DC-FAN/</a><br>
If so, it looks like these are ball-bearing (the -PHB- in the model number would be -PHS- if it were a sleeve bearing). Maybe. The data sheet is awfully brief and is partly in Chinese, which I can't read.</p>
PresidentOfAwesomeness on COM-09649 - DC Brushless Fan - 80x80x15mm (5V)PresidentOfAwesomenessurn:uuid:2faad016-cce7-c854-8353-54bff3ec062b2010-02-20T06:58:46-07:00<p>Also an important thing to know would be if these are ball bearing or sleeve. I would guess sleeve bearings, because of the price, but I'm just making sure. (These are important things to know, please tell us!)</p>
PresidentOfAwesomeness on COM-09649 - DC Brushless Fan - 80x80x15mm (5V)PresidentOfAwesomenessurn:uuid:f8a10d63-df0f-e517-c8a7-14eeeef7213e2010-02-19T13:59:47-07:00<p>Uh... how much air can these fans move (CFM)?</p>