SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-18T19:07:56-06:00SparkFun ElectronicsCustomer #27577 on DEV-09709 - ProtoShield for Arduino Pro MiniCustomer #27577urn:uuid:ccf02db2-4a13-508b-8c5d-9f9d3c734c7b2012-11-05T17:56:18-07:00<p>That would be a much better design. Please do the above.</p>
IllogicGate on DEV-09709 - ProtoShield for Arduino Pro MiniIllogicGateurn:uuid:fce0ec50-214a-fcf3-9381-0d86456d11f22012-08-15T14:05:04-06:00<p>This will be very useful for my RoWD (Robot of World Domination)... Muhahahaha! >:D</p>
sudopeople on DEV-09709 - ProtoShield for Arduino Pro Minisudopeopleurn:uuid:37f693a9-20ca-787d-2b07-400f28dbbb062012-02-02T11:57:42-07:00<p>SparkFun: On the next round of these, please do <a href="http://i.imgur.com/4bV12.jpg" rel="nofollow">this</a>.<p>Note the bused I/O pins for easy connection to sensors.</p></p>
Customer #27577 on DEV-09709 - ProtoShield for Arduino Pro MiniCustomer #27577urn:uuid:b8e29fc4-ad8c-b6fb-1d0c-b1d165fa97002011-12-05T21:29:29-07:00<p>I second that. I was surprised it wasn't designed like that to begin with.</p>
Microman on DEV-09709 - ProtoShield for Arduino Pro MiniMicromanurn:uuid:b41c935f-cf2e-ac2d-ccdb-0bdbf4d5572d2011-08-23T10:23:11-06:00<p>I Agree. a newer design of this board (hopefully) should allow you to create shields that can be simple mounted via headers onto all the pro mini pins, making it a true protoshield</p>
Customer #217718 on DEV-09709 - ProtoShield for Arduino Pro MiniCustomer #217718urn:uuid:2db1b51c-3589-8055-b8ec-79640cd18c4d2011-05-22T17:57:20-06:00<p>I need to use the (offset) A4 and A5 pins on the ProMini but haven't figured out how to bring these up to the shield - which I will later need to be able to remove. Would the Arduino offset headers (mounted upside-down on the shield) match the spacing? Has anyone done something like this successfully?</p>
littlefreak on DEV-09709 - ProtoShield for Arduino Pro Minilittlefreakurn:uuid:5abc6f7d-4779-8e75-b56e-4947041bc9182011-04-28T08:07:04-06:00<p>Wish it connected to all pins on the mini. So I could by multiple for prototyping and then just swap my mini between projects. With this set up I'll still have to solder directly to the mini to reach any of the inputs.</p>
Customer #165462 on DEV-09709 - ProtoShield for Arduino Pro MiniCustomer #165462urn:uuid:3104f2a6-7aca-0827-10ac-a13e036e982b2011-01-11T13:46:54-07:00<p>Is this compatible with the Arduino Stamp?</p>
myHalici on DEV-09709 - ProtoShield for Arduino Pro MinimyHaliciurn:uuid:ac3b12ed-412c-f8b7-6867-b0ab69707a4c2010-04-03T19:39:00-06:00<p>Eagle files?</p>
Jamo on DEV-09709 - ProtoShield for Arduino Pro MiniJamourn:uuid:f089ba47-f64e-3e78-c96f-d2fd4a0736882010-04-02T00:39:43-06:00<p>Can we get something like this for the FIO?</p>
azrobbo on DEV-09709 - ProtoShield for Arduino Pro Miniazrobbourn:uuid:0f82aa39-2e33-2599-e72f-e1c0a5e4a0ae2010-03-31T17:47:21-06:00<p>Cool new product.<br>
Sparkfun is genius at creating new "must have" items that we didn't even know we needed.</p>