SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T23:23:12-06:00SparkFun ElectronicsHmmm on CAB-09741 - IC Hook with PigtailHmmmurn:uuid:5bb3644b-5583-49e6-79d3-6f6862a884372014-04-08T12:22:39-06:00<p>They can grab a single SOIC pin, but the plastic head is so big you can only probe one at a time, not 2 adjacent ones.</p>
Customer #336404 on CAB-09741 - IC Hook with PigtailCustomer #336404urn:uuid:6cccf6f9-c683-a304-3173-27306f5fce3d2013-08-03T14:08:12-06:00<p>These IC clips to pigtails are great for testing .. I have used for my breadboard to connect power and also to test my servos, the pigtail pins fit great into the servo plugs. Great stuff I will share it with my other friends who love this stuff as much as I do.</p>
cmat on CAB-09741 - IC Hook with Pigtailcmaturn:uuid:92c204f9-f69b-cc93-d923-5ffdd5c736bd2013-05-15T19:10:56-06:00<p>Quite useful for hooking up parts I want to test and not damage by soldering leads.</p>
RoiLorelai on CAB-09741 - IC Hook with PigtailRoiLorelaiurn:uuid:04b79199-5c0d-6284-34fa-c9863f65e9572012-02-29T01:42:44-07:00<p>Lucky me... just saw the stock dry up ;)</p>
bhunting on CAB-09741 - IC Hook with Pigtailbhuntingurn:uuid:92a085bb-aa80-ced5-a710-a3d1b1e433172010-08-23T22:36:38-06:00<p>dave2, "description suggests only huge packages" is reasonably accurate. I'm sitting here with a package of these in my hand. I'd say they will be good for 0.1 headers, solderless breadboard work, passive lead clipping, standard dips, meaty connection points like that. I don't expect these would do well with fine pitch ICs. These are NOT micro-grabbers. At $5 for 5 don't expect them to be.</p>
dave2 on CAB-09741 - IC Hook with Pigtaildave2urn:uuid:ec89d18c-c59d-7b22-c889-ad702abd06432010-06-07T21:39:19-06:00<p>Any idea how fine these can tap single IC pins? Looking for something which can cope with at least 0.8mm pitch TQFP. Bonus points if it can live with 0.65mm SSOP or 0.5mm TQFP.<br>
SOIC in description suggests only huge packages.</p>