SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T12:12:01-06:00SparkFun ElectronicsCustomer #888745 on COM-09773 - Fuse Clip 5mmCustomer #888745urn:uuid:26c97b85-c663-9129-7fc9-e10e1eccfa732017-12-14T06:34:29-07:00<p>Regarding selling them in pairs, if you break or lose one (or any other odd number) you wouldn't need an even number of replacements. So selling any number provides the best flexibility for the buyer.</p>
JerZ on COM-09773 - Fuse Clip 5mmJerZurn:uuid:5dca5ef6-880d-cc2d-9a7c-a61b75f497852013-08-11T19:54:29-06:00<p>These are great little motor mounts for 6mm pager motors, if your into building little robots and such. They clip right in just like a fuse would.</p>
Tom VdA on COM-09773 - Fuse Clip 5mmTom VdAurn:uuid:5ceffe99-f21f-27ff-367a-4ff1dce0f3a72013-01-24T15:08:52-07:00<p>is there a fritzing part for this item?
i'm not sure how to place it on a pcb so it will fit the hole...</p>
Nate on COM-09773 - Fuse Clip 5mmNateurn:uuid:bb92ffc4-1dc3-e895-26b1-f28d1ad972432010-05-06T17:07:05-06:00<p>Good point. Part# added: 1A3399-10</p>
esklar81 on COM-09773 - Fuse Clip 5mmesklar81urn:uuid:8f04763b-1773-fa12-d1a7-c5cf5c23564f2010-05-04T22:16:27-06:00<p>SparkFun Folks.<br>
1) Which Buss part number is this? There are quite a few on the attached datasheet. (Please add specifying the manufacturer's part number to your procedure for writing catalog pages, at least when you provide a datasheet that contains more than one part.)<br>
2) Wouldn't it make more sense to sell these in pairs? There's not a lot of uses for a single fuse holder.<br>
TIA,<br>
Eric</p>