SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-29T00:15:02-06:00SparkFun Electronicscoonce on RTL-09875 - RFID Starter Kit - Retailcoonceurn:uuid:27f350d6-2c9e-296c-65c2-9b839990bbe42012-11-28T22:52:04-07:00<p>So... is this product currently sold out?<p>If so, will you guys be making any more?</p><p>If not, is there another product that's similar in scope?</p></p>
Customer #371260 on RTL-09875 - RFID Starter Kit - RetailCustomer #371260urn:uuid:6bda79ec-495a-11b5-d642-a9205e13301e2012-10-19T03:51:42-06:00<p>Truly excellent piece of kit. No duino required and Very easy too connect to. A small tip for those strugling with HyperTerm tools osx/pc, you can also use the default Arduino SerialMonitor to monitor other COM ports too. Just switch the COM tool=>serial port, and open the serial monitor.<p>For thos who want to connect with Arduino to the Serial port on the board instead of USB FTDI.</p><p>Here's my code:
http://pastebin.com/rWhJ7aRy</p></p>
Customer #368590 on RTL-09875 - RFID Starter Kit - RetailCustomer #368590urn:uuid:dfd54fd1-7394-ca61-c674-575eacb899182012-10-16T11:02:14-06:00<p>Is there any application you know of that is similar to Powerwedge http://www.carabez.com/pcwedge.html that can be used for Mac's?</p>
Customer #288577 on RTL-09875 - RFID Starter Kit - RetailCustomer #288577urn:uuid:70cdd227-9b18-c572-31ba-78f71d4cd2262012-10-15T18:00:48-06:00<p>I have problems with this module, I wired it in with an arduino uno and an LCD display, and the read LED keeps flashing and the buzzer buzz's on and off, both very fast.
can anyone help?</p>
UNTEngineer on RTL-09875 - RFID Starter Kit - RetailUNTEngineerurn:uuid:69b5265e-5968-293e-9450-6ff927a981962012-08-30T18:29:30-06:00<p>Can this work on 3.3V say for use with an Arduino Fio?</p>
mctom987 on RTL-09875 - RFID Starter Kit - Retailmctom987urn:uuid:cf2726d7-08b0-4320-daff-db6962b30ae92012-07-06T22:56:25-06:00<p>This kit is far superior to another one I bought at Fry's (Parallax).
I spent a couple hours trying to avoid duplicating (ok, centicating) successive reads. This device has that built in, so I no longer have to fudge around in my code to only check once. Great job!<p>The built-in beep is also a nice addition. Were it not useful to have two readers, I'd likely return the Parallax one.</p></p>
heavysixer on RTL-09875 - RFID Starter Kit - Retailheavysixerurn:uuid:ce4d6698-063b-233c-34c9-dd6f65c1e4ad2012-04-23T09:58:24-06:00<p>I wrote a short blog post on how to get this working with the Mac and Ruby: http://markdaggett.com/blog/2012/04/23/reading-rfid-cards-with-ruby/</p>
Customer #129248 on RTL-09875 - RFID Starter Kit - RetailCustomer #129248urn:uuid:9eba571c-6608-1a1b-795e-a7bcfaebe9432012-04-03T16:20:47-06:00<p>Hello,
I bought this kit and it's working fine.<p>But a have a need to know when the card get away from the reader. How can I do that? I imagined try to read the card each 1 second, but I don't know what command to send to the reader to do that.</p><p>Some one knows how can I do?</p><p>Best regards.
Thiago</p></p>
Marabunta on RTL-09875 - RFID Starter Kit - RetailMarabuntaurn:uuid:e36b1a1a-e842-2bc9-e8e2-5e11c13312932012-02-12T14:02:03-07:00<p>Hello,
How can I copy or echo the data read by TeraTerm to microsoft access 2011? Hope that someone can help me!
Thnx, Marabunta</p>
Mike N. on RTL-09875 - RFID Starter Kit - RetailMike N.urn:uuid:49f6acf8-cfe7-140a-f212-d312dd0091522012-02-10T16:09:00-07:00<p>Has anyone been able to get this reader to be able to log into windows?</p>
ITHelp on RTL-09875 - RFID Starter Kit - RetailITHelpurn:uuid:5e2e2a70-869d-3487-1c05-5b72691f54a22011-12-09T12:53:43-07:00<p>If you are looking for cards that you can set the values of then look into the MIFARE module and tags.<p>These tags are set at the factory and cannot be edited later on. The readers are not capable of writing to tags anyways, but there are read/write modules that operate in the 125 kHz range, given the proper tags.</p></p>
ITHelp on RTL-09875 - RFID Starter Kit - RetailITHelpurn:uuid:91a57602-fefa-cd7f-cae5-5c8ffb8793832011-12-09T12:51:24-07:00<p>Make sure you've set your connection up properly. This module outputs at 9600 baud, not 115200.<p>Beyond that it's 8N1N (8 data bits, no parity, 1 stop bit, no flow control.)</p><p>The tutorial steps you through the HyperTerm setup. http://www.sparkfun.com/tutorials/243</p></p>
ITHelp on RTL-09875 - RFID Starter Kit - RetailITHelpurn:uuid:2b9bbe19-258c-1826-8dce-8a4bd4b69a562011-12-09T12:49:00-07:00<p>Unfortunately there is not. The output is the raw data from the tag, so you can convert that to binary and work back up if you need to get different values from various ranges in the card's output.<p>(It comes from the reader in hexadecimal format, so it's a fairly straightforward conversion to binary.)</p></p>
ITHelp on RTL-09875 - RFID Starter Kit - RetailITHelpurn:uuid:2a9ad2ec-ddca-b42a-b272-420beeb76e592011-12-09T12:46:40-07:00<p>Yes. You actually need to tie FS (Format Select) to GND and RST to VCC as well. All told it only takes three lines from the Arduino to run it.<p>EDIT: I use the NewSoftSerial library to read from this as well. It works great and it leaves the hardware UART open for other uses.</p></p>
@maxboender on RTL-09875 - RFID Starter Kit - Retail@maxboenderurn:uuid:5dfa652a-c1ee-502f-c911-4d2c6d5048272011-12-04T02:07:13-07:00<p>I used the tutorial but hyperterminal only shows triangles. What do i do?</p>
tomdavies on RTL-09875 - RFID Starter Kit - Retailtomdaviesurn:uuid:4a893b58-6ea5-6109-2890-a79805d4d8b22011-11-19T14:47:52-07:00<p>Is it possible to run this with just the uno by connecting up the vcc, ground and tx pins??</p>
TQT on RTL-09875 - RFID Starter Kit - RetailTQTurn:uuid:78561c9c-b154-ef80-6c35-3eb2facfe8ad2011-10-30T15:30:39-06:00<p>In case you haven't resolved it yet, just use the TX and RX lines and read it as any other serial device.</p>
Jippie on RTL-09875 - RFID Starter Kit - RetailJippieurn:uuid:7d317f2b-00c7-d8bb-6e23-2730ecaac0672011-10-24T09:21:18-06:00<p>Hello,<br>
The link to the Quick Start Guide doesn't seem to work. I'm working on a Mac. Can somebody give me quick start :)?...<br>
best,<br>
Jippie</p>
CarlosNegron on RTL-09875 - RFID Starter Kit - RetailCarlosNegronurn:uuid:cf69ec19-d64c-c39e-311c-3a61bb2347d32011-08-04T20:44:34-06:00<p>is there anyway to change the output data format?</p>
Customer #241469 on RTL-09875 - RFID Starter Kit - RetailCustomer #241469urn:uuid:d889f3ac-5333-6a34-1c9b-49cf4cc44f992011-07-31T18:37:08-06:00<p>I have the some doubt!</p>
Customer #241469 on RTL-09875 - RFID Starter Kit - RetailCustomer #241469urn:uuid:af9e2c75-e057-4586-713f-a83e7c87f0bf2011-07-31T18:36:29-06:00<p>Is there a way to connect the RFID USB Reader to the Arduino UNO?</p>
CarlosNegron on RTL-09875 - RFID Starter Kit - RetailCarlosNegronurn:uuid:981b2e47-c31a-fe1f-9931-78a7104e9adb2011-07-07T23:02:23-06:00<p>Recently i purchased this item along with the REDBEE (125khz) to use them on my thesis project. The problem is that when i read the cards using the Windows Hyperterminal, it shows a diferent code using this item and the REDBEE, all of this with thbe same rfid tag. Does anyone know how to fix that? thanks</p>
Customer #231857 on RTL-09875 - RFID Starter Kit - RetailCustomer #231857urn:uuid:0b3b558b-5572-04a3-b08a-f61a1d1a8b042011-06-12T17:19:26-06:00<p>Hello<br>
I want to use this product for connecting with altera de2 board.This development board has ps/2, rs 232 and also usb port. can somebody give me any idea?</p>
Customer #225883 on RTL-09875 - RFID Starter Kit - RetailCustomer #225883urn:uuid:cbee6b63-bd95-d2cf-f13f-3fc946b9168f2011-05-16T07:39:14-06:00<p>How did your project go? Please contact me, i think my email should be visible here :s</p>
Customer #218560 on RTL-09875 - RFID Starter Kit - RetailCustomer #218560urn:uuid:21d3543a-f1cc-58e9-f336-29bf85bf0ec22011-05-10T08:39:48-06:00<p>Is there a way to connect the included RFID USB board to the Arduino Pro board?</p>
Customer #63087 on RTL-09875 - RFID Starter Kit - RetailCustomer #63087urn:uuid:3d3e6479-3571-4325-2c75-967ce903f5062011-05-01T07:14:55-06:00<p>Hi,<br>
I have tags rewritables (T5567 type) - which I can read in this module ok.<br>
Can I use this module also to write to this tags?<br>
(I can write to TAGS with another readder/writer I have)<br>
Are there any commands - to to the writing?, any datasheet how to use this module for writing?<br>
Is it possible at all with the ID-12?<br>
please email me to<br>
roeebloch@walla.co.il<br>
Thanks,<br>
Roee.</p>
Toni_K on RTL-09875 - RFID Starter Kit - RetailToni_Kurn:uuid:aeaf0c55-23b0-2293-96fa-52cdfecc43b22011-04-28T12:22:24-06:00<p>To get accurate results, you will need a 134kHz reader to read 134kHz transponders. You may be able to pick up the occasional 134kHz module with 125 kHz module, but this is the exception rather than the rule. You could hack the USB reader to be compatible with a 134kHz module, but it is currently only designed for the ID-2, ID-12 and ID-20 modules. It would probably be easier to simply build your own reader interface board for whatever module you would like to use.</p>
coudcoud on RTL-09875 - RFID Starter Kit - Retailcoudcoudurn:uuid:aec050f0-f6b1-595a-10ea-fc2bb8389aac2011-03-21T14:57:27-06:00<p>Hello.<br>
I wanted to build a 134khz rfid reader, to use it with animal ear tags.<br>
I read that some 125khz readers could view 134khz transponders.<br>
However it doesn't seem to work with an out-of-the-box rfid starter kit.<br>
I'm a beginner in electronics, so I don't know if there is a way to change/add a component in the "RFID USB reader" in order to change the reading frequency.<br>
Is it hackable?<br>
Thanks.</p>
Customer #209796 on RTL-09875 - RFID Starter Kit - RetailCustomer #209796urn:uuid:52700b1d-14c4-5f4a-22bd-536c3c140c162011-03-11T18:34:54-07:00<p>Hello thr,<br>
I m gonna use this device along with my java project. So I require the Java SDK along with starter pack.<br>
Plz let me ensure that Java SDK would be there along with the device. So that I can start with my project.<br>
Thnx</p>
Young Maker on RTL-09875 - RFID Starter Kit - RetailYoung Makerurn:uuid:6ef537b5-23c0-b66d-39b8-36e0dcb58dff2011-02-26T13:31:41-07:00<p>no because they are factory set cards. you may only read them.</p>
camigord on RTL-09875 - RFID Starter Kit - Retailcamigordurn:uuid:3887cc4d-5400-4ce9-66e2-cf969ef6603b2011-02-24T18:18:06-07:00<p>sorry, is there any way to write the card? or it has a unique ID? Thanks</p>